STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Whether the size of FSBL is limited to one block of NAND, and shell we tailor the FSBL(tf-a) within 128KB to fit MT29F4G08,which block size is 128KB?

Hello, we are using a NAND Flash MT29F4G08 as boot device, which block size is 128KB. We program the 245KB size of FSBL(tf-a.stm32) to it with cubeProgrammer successfully, it does not boot up. When we replace the NAND Flash with MT29F8G08 as boot dev...

SunnyGeGe by Associate III
  • 3054 Views
  • 5 replies
  • 0 kudos

ST32MP157C-DK2 low power operation

I've been trying to reduce power consumption of the STM32MP157C-DK2 board and have a very low power linux platform. But the power consumption seems somewhat agnostic of power rails and clock rates. For example, I removed the LCD, I boot to u-boot, th...

nlbutts by Associate II
  • 1791 Views
  • 1 replies
  • 0 kudos

Resolved! Using ST Yocto SDK with Docker for Windows

Hi,I've been trying to setup a cross compile environment using Docker for Windows, and I've run into a bit of trouble. I've setup the dockerfile so that during the build process of the image, I copy the SDK into the image and execute the .sh script.T...

TOlli by Senior
  • 4566 Views
  • 7 replies
  • 0 kudos

Moving LTDC pins on DK2 board?

Just wondering if I can edit the pinctrl.dsi file to change the pins to the Raspberry Pi header, rather than the HDMI encoder, so I can try DPI Raspberry Pi displays. In CubeMX the LTDC and most of the peripherals are locked, just wondering if it is ...

AJaro.2 by Associate II
  • 2949 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.