STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Display in separate module

Lets say I need to separate module, one will contain the pcb with mpu and other IC, the second will contain a touchscreen display and sensors. The modules are 2 meters apart. What should I use hdmi or mipi? How do I send mipi over distance?

GEspi.19 by Associate
  • 1072 Views
  • 1 replies
  • 0 kudos

Reliability of M4 and A7 through RPMSG

I wrote an application on the STM32MP157C-DK2, and m4 reads the data of an external adc and sends it to A7 for processing. The entire program got stuck after running for about 15 hours. The console has been outputting the following content[84306.5118...

Jzhua by Associate III
  • 2109 Views
  • 4 replies
  • 0 kudos

Imaging the provided SD Card

I'm trying to image the provided SD Card. I'm trying to use `dd` but it seems to only be cloning about 33mb before saying it is finished with no other output. sudo dd if=/dev/disk2 of=~/stmicro.imgAny thoughts?

JSlac by Associate II
  • 1953 Views
  • 2 replies
  • 0 kudos

Issue with running from SRAM

This is a new issue involved in running from SRAM. I recently posted an issue:https://community.st.com/s/question/0D50X0000BDnc5pSQB/stm32f7-uart5-issueand this is a second, possibly related issue.The software I am writing is a Built-in-Test and boot...

SBurc by Associate II
  • 1537 Views
  • 1 replies
  • 0 kudos

Resolved! FMC with NOR FLASH memory

Hi,I'm trying to reserve the pins for FMC that would be connected to NOR FLASH. The STM32CubeMX will give me some of the pins, mainly the data lines (FMC_D0:FMC_D15) for 16 bit data.Since the reference manual states that FMC has to be configured afte...

TOlli by Senior
  • 2989 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.