STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! data exchange OpenAMP_TTY_echo

Hello,I am reimplementing the example application OpenAMP_TTY_echo in STM32MP157C-DK2.I want to exchange numerical data between M4 and dual A7. How can I do it ? which structure, channel or interface ?thanks in advance

IYetk by Associate III
  • 2108 Views
  • 4 replies
  • 0 kudos

why the system workbench use stklink?

Hi, I use system workbench to debug example project. The serial port and ethernet over usb are recognized by system workbench. Now, the debuger step is using openocd to connect target board. I follow the below link to setting the debug configuratio...

0690X0000097zpKQAQ.png
SChen.11 by Associate III
  • 2343 Views
  • 4 replies
  • 0 kudos

STM32MP157 software problem

The software of the company is developed based on QT framework. Due to some limitations of the framework, opengles cannot be better used. Can you use linuxfb to run QT program?I can't find the /dev/fb0 interface:grinning_face:

Yli.8 by Associate II
  • 1325 Views
  • 1 replies
  • 0 kudos

M4 GPIO realistic maximal frequency ?

How long does it take (approx) to rise or lower a GPIO pin fix configured to the M4 in the STM32MP157c, after issuing the command in the M4 code ? On our native STM32F409 board it takes around 10ns. I'm afraid the STM32MP1xx is much slower right ? Re...

DBuer by Associate II
  • 1758 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.