2020-01-06 2:49 AM
Hello,
we would like to boot from a eMMC memory on our board connected to SDMMC2.
As the camera interface is in conflic with SDMMC2 8bit mode, we must configure it as a SDMMC 4 bit width.
The question is will we still me able to boot from our eMMC memory in 4 bit mode as we do in 8 bit ?
The memory we use is the following MTFC4GACAJCN-1M from Micron
Tanks for your support.
2020-01-06 2:58 AM
At HW level, there is no issue to use 4-bit eMMC as BootROM first boot level only use one data line, e.g. CLK/CMD and D0 on PE3/PG6 and PB14 (see AN5031).
To restrict usage to 4-bit eMMC in TF-A and uBoot/Linux, you should adapt the Device Tree.
Please note that we currently have a limitation for eMMC boot from Micron devices, see ES0438. Meanwhile you should use Toshiba or Kingston devices. This will be solved in future silicon.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.