2020-01-06 2:18 AM
Hello, I'd like to install Python dependencies to run a RTL-SDR python program on the discovery kit and I failed to execute the following command line below :
apt-get install python-numpy (or python3-numpy).
Do you know how to install numpy on the DK2 ?
BR
2020-01-06 5:35 AM
Hi @JDUMA
apt-get service is not yet available for OpenSTLinux, it will come with next V1.2.0 release in February this year.
In the meantime, actually python3-numpy is already part of the Distribution package but not compiled and installed by default.
2 ways to install it on target, the complete/proper one :
Adding it to RDEPENDS_packagegroup-framework-tools-python3 variable in layers/meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools.bb and rebuild the full image and reflash it on the DK2.
one shortcut for a try :
do "bitbake python3-numpy"
The generated debian package will be available in : tmp-glibc/deploy/deb/cortexa7t2hf-neon-vfpv4/
Copy it on target and install it with dpkg -i python3-numpy*.deb
Hope it help
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.