STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! PMIC-related issues

The STM32MP135 is powered by PMIC1A. After initial power-up, the voltage at BUCK4 is normal at 3.3V, but during U-Boot flashing, the output voltage at VOUT4 drops to only 2.4V, causing the flashing to fail. The VDD and VDDQ pins of the eMMC are power...

LH1 by Associate II
  • 316 Views
  • 1 replies
  • 0 kudos

MIPI DSI IBIS MODEL for STM32MP255

Hi, I tried exporting the IBIS model from ST website. On importing model to SI tool I can see that there is no model assigned to DSI lines. It is showing NC. Can you share the IBIS model with MIPI drivers in it. or share some IBIS model which I can u...

DJ_IND_0-1758102381709.png
DJ_IND by Associate III
  • 896 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.