STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! DSI display comes up during U-Boot and displays ST Logo but turns off once Linux Kernel takes over on our custom DK2 board. Weston Wayland Compositor fails to start during boot and backlight setup fails too. Does Wayland compositor have GPIO dependencies?

Most of the DSI pin mapping is same as ST's DK2 board except DSI_RESET and DSI_TE. I updated the DSI_RESET pin mapping in the device tree to reflect actual connections. However, Weston Wayland compositor fails to start even when DSI display is not co...

EB.1 by Associate II
  • 4177 Views
  • 3 replies
  • 0 kudos

hello.We design a board based on ev1,we use silicon image rgb/hdmi bridge ,but it dosen't display on moniter

 sii902x 1-0039: Linked as a consumer to regulator.3[  2.001069] sii902x 1-0039: Linked as a consumer to regulator.4modetest -M stmEncoders:id   crtc  type  possible cstcs possible clones28   31   D@I   0x00000001   0x00000000Connectors:id   encoder ...

Cliqi by Associate
  • 1704 Views
  • 2 replies
  • 0 kudos

Uboot DFU not working

We have build a device that looks like DK2 but we have a NAND memory instead of SD card and we work on an IO supply of 1.8V instead of 3.3V. We can load the fsbl and U-Boot with STM32cubeprogrammer, but U-Boot resets the usb and the STM32cubeprogramm...

JVerb.1 by Associate II
  • 4528 Views
  • 9 replies
  • 1 kudos

Resolved! Copy file into bootfs partition

Using the Distribution Package for STM32MP1 I wrote a simple function to copy some file to the rootfs image and execute fine-tuning commands:my_postprocess_function() { cp -dr /home/osboxes/Documents/overlay/* ${IMAGE_ROOTFS} ln -s /lib/systemd/sys...

Mark81 by Associate III
  • 1678 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.