2020-03-11 8:58 AM
Hi all,
If I dedicate the MCU SRAM2 for data and MCU SRAM4 for DMA as shown here, do I get CCM like performance or do I have a risk to have contention on the SRAM2 ?
After looking at the bus matrix, I suspect there is no risk but I want to make sure it is the case.
Solved! Go to Solution.
2020-03-11 10:09 AM
I confirm there is no contention in the MLAHB matrix, e.g. in your case between Cortex-M4 and SRAM2 and DMA access to SRAM4.
For information, to get best performances for Cortex-M4 DATA access, either RETRAM (@0x00000000, using D-Bus) or SRAM2 alias (@0x30020000, using S-Bus) should be used (other SRAMs have still good performances, but could have 1 additional wait-state on non-sequential access from Cortex-M4). Notice that Cortex-M4 INSTRUCTION fetch is 'optimized' on either S-bus or I-bus on all SRAMs and RETRAM (even if I-bus should be preferable).
2020-03-11 10:09 AM
I confirm there is no contention in the MLAHB matrix, e.g. in your case between Cortex-M4 and SRAM2 and DMA access to SRAM4.
For information, to get best performances for Cortex-M4 DATA access, either RETRAM (@0x00000000, using D-Bus) or SRAM2 alias (@0x30020000, using S-Bus) should be used (other SRAMs have still good performances, but could have 1 additional wait-state on non-sequential access from Cortex-M4). Notice that Cortex-M4 INSTRUCTION fetch is 'optimized' on either S-bus or I-bus on all SRAMs and RETRAM (even if I-bus should be preferable).
2020-03-12 1:19 AM
Hi @PatrickF ,
Thanks for the detailed explanation.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.