STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP157C-DK2 maximum current 5V/3V3 pins

Hi,I want to connect some shields/sensors to STM32MP157C-DK2. Some of the sensors will draw about 200mA. How much current can I draw from the 5V/3V3 pins on the GPIO expansion connectors? The STM32MP157C-DK2 is powered over USB-C 5V/3A. OpenSTLinux i...

Lukas1 by Associate III
  • 1337 Views
  • 1 replies
  • 0 kudos

Resolved! OpenAMP hangs at MX_OPENAMP_Init() when started from U-Boot, even after waited for linux to fully booted up.

When I run the openamp image through linux command prompt, the application working fine. The RPMSG devices is created successfully.But when I've tried to run it from uboot, it stuck at MX_OPENAMP_Init(). This should be ok because I assume linux isn't...

Resolved! TFA boot failed with emmc flash

Hi, I has two custom boards. There are have same stm32mp157 ic and ddr. The difference is emmc flash, A's from micron and B is THGBMNG5D1LBAIL. Basic chain:The A and B are bootup success.Trusted chain(TF-A + U-Boot)The A is bootup success.The B is bo...

SChen.11 by Associate III
  • 3823 Views
  • 4 replies
  • 0 kudos

First steps with STM32MP1

Hello everyone.I am introducing me on this world of multiprocessors, by the moment I only had worked with NUCLEO-F3 boards or similar.For my new research, I plan to purchase a SOM + Carrier board with the STM32MP157C microcontroller.My intention is t...

JTant.1 by Associate II
  • 2579 Views
  • 4 replies
  • 0 kudos

We see dull colours on our LCD, using "modetest" on our custom board, while the colours are bright when the same LCD hangs on the DK2. Are there possible causes we could check? Colour space, gamma correction?

We have made a custom board with an STM32MP157CAD MPU, this board is very similar to the DK2. We have adapted an LCD driver to support our LCD screen, over the DSI interface. It works, both on the DK2 with our own LCD screen, and on our custom board ...

OL'He.1 by Associate III
  • 1194 Views
  • 0 replies
  • 0 kudos

Getting Started with MIPI DSI Display

Hello,I am fairly new to Linux and am trying to drive a DSI display using the STM32MP15-DK2 (not the one that came with the board) and was looking for some direction. I have been reading through the documentation related to DSI such as the DSI Intern...

BSunw.1 by Associate III
  • 3385 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.