2020-03-30 1:39 AM
hello all
i have a STM32MP157C-EV1, and I want to build an m4 core development and debugging environment in minimal "st-image-core".
M4 firmware created using "STM32CudeIDE" can be debugged in "st-image-weston", but an error occurs in "st-image-core".
What items should be added to "st-image-core.bb" to work normally?
error message :
[ 100.552483] remoteproc remoteproc0: powering up m4
[ 100.555897] remoteproc remoteproc0: Direct firmware load for OpenAMP_TTY_echo_CM4.elf failed with error -2
[ 100.571270] remoteproc remoteproc0: request_firmware failed: -2
[ 100.575829] remoteproc remoteproc0: Boot failed: -2
I will wait for your reply.
Solved! Go to Solution.
2020-04-06 5:49 AM
Hi @Machilus
I can not figure out why remote proc browse so many folders ?
What is the structure of the /lib/firmware on your target ?
Where /lib/firmware/updates/4.19.94/ come from ?
Where is the OpenAMP_TTY_echo_CM4.elf exactly before you start the firmware ?
If I got it right it's working with "st-image-weston". Can you share the succeeded trace of firmware start ?
Any difference in /lib/firmware folder structure ?
Hope it help,
Olivier
2020-03-30 2:33 AM
Hi @Machilus ,
By comparing with st-image-weston.bb, I guess adding "eclipe-debug" in IMAGE_FEATURES looks to be good candidate.
I will ask for confirmation from expert.
Does your traces come from a Debug session from STM32CubeIDE or a manual start of firmware from Linux ?
Olivier
2020-03-30 5:14 PM
^^:
2020-03-31 5:26 PM
Hi @OlivierG (ST Employee)
Thank you for your reply.
Tracking is a kernel message when executing a debug session of "STM32CubeIDE".
Adding "eclipse-debug" to "st-image-core.bb" has not solved the problem.
IMAGE_FEATURES += "\
package-management \
ssh-server-dropbear \
eclipse-debug \
"
2020-04-01 1:33 AM
Hi @Machilus
Your initial trace show an error due to fact that firmware is missing in /lib/firmware
STM32CubeIDE is using ethernet connection to copy the .elf to the target.
Ethernet service may likely miss in st-image-core ( check on going at my end)
Did you noticed something wrong during download of .elf with STM32CubeIDE ?
Could you try manual copy and start of firmware on target using this
Thanks for feedback
Olivier
2020-04-02 2:38 AM
Hi @OlivierG (ST Employee)
No download problems using "STM32CubeIDE".
When manually running firmware in the manner OlivierG suggested,
the following problems occurred.
<< Execution Message >>
root@stm32mp1-fiscal:/lib# echo start >/sys/class/remoteproc/remoteproc0/state
[ 1090.457191] remoteproc remoteproc0: powering up m4
[ 1090.460584] remoteproc remoteproc0: loading /lib/firmware/updates/4.19.94/FISCAL_CM4.elf failed with error -20
[ 1090.474820] remoteproc remoteproc0: loading /lib/firmware/updates/FISCAL_CM4.elf failed with error -20
[ 1090.484713] remoteproc remoteproc0: loading /lib/firmware/4.19.94/FISCAL_CM4.elf failed with error -20
[ 1090.494670] remoteproc remoteproc0: loading /lib/firmware/FISCAL_CM4.elf failed with error -20
[ 1090.503785] remoteproc remoteproc0: Direct firmware load for FISCAL_CM4.elf failed with error -20
[ 1090.511210] remoteproc remoteproc0: request_firmware failed: -20
[ 1090.520436] remoteproc remoteproc0: Boot failed: -20
<<Below is a message from OpenOCD using ST-LINK.>>
Open On-Chip Debugger 0.10.0+dev-01193-g5ce997d (2020-02-20-10:54)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
cortex_a interrupt mask on
cortex_a interrupt mask on
cortex_a domain access control fixup on
cortex_a domain access control fixup on
none separate
adapter speed: 8000 kHz
adapter_nsrst_assert_width: 200
adapter_nsrst_delay: 200
none srst_pulls_trst
srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V3J6M2B4S1 (API v3) VID:PID 0483:374F
Info : using stlink api v3
Info : Target voltage: 3.238171
Info : clock speed 8000 kHz
Info : SRST line released
Info : stlink_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : STM32MP151CAAx.cpu0: hardware has 6 breakpoints, 4 watchpoints
Error: Could not find MEM-AP to control the core
Info : Listening on port 3334 for gdb connections
Info : Listening on port 3333 for gdb connections
ap 0 selected, csw 0x10006000
Info : accepting 'gdb' connection on tcp/3333
Error: Target not examined yet
Info : New GDB Connection: 1, Target STM32MP157CAAx.cpu2, state: unknown
undefined debug reason 7 - target needs reset
Error: Target not examined yet
Error: Target not examined yet
Error: Target not examined yet
Error: Target not examined yet
Thank you for your interest in this problem.
2020-04-02 3:02 AM
Hi @Machilus
I noticed very strange/abnormal traces in your OpenOCD log :
Info : STLINK V3J6M2B4S1 (API v3) VID:PID 0483:374F
Info : STM32MP151CAAx.cpu0: hardware has 6 breakpoints, 4 watchpoints
Definitly not matching an EV1 board !?
Can you clarify your setup ?
For which target did you compile the .elf ?
For manual start of firmware can you confirm the firmware is well present in /lib/firmware ?
Thanks
Olivier
2020-04-03 1:26 AM
Hi @OlivierG (ST Employee)
Sorry.
I sent the wrong message.
It was a message from a custom board made from a "STM32MP151C" chip based on the "STM32MP157C-EV1" board.
Recently, I debugging "OpenAMP_TTY_echo" firmware from created a "st-image-core" distribution on the "EV1" Board.
It worked without error.
However, running the M4 firmware on the custom board based on "STM32MP151C" resulted in an error.
This error does not occur in the "st-image-weston" distribution,
Error occurs only in "st-image-core" distribution.
<<Below is a message from OpenOCD using ST-LINK V3SET>>
Open On-Chip Debugger 0.10.0+dev-01193-g5ce997d (2020-02-20-10:54)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
cortex_a interrupt mask on
cortex_a interrupt mask on
cortex_a domain access control fixup on
cortex_a domain access control fixup on
none separate
adapter speed: 8000 kHz
adapter_nsrst_assert_width: 200
adapter_nsrst_delay: 200
none srst_pulls_trst
srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V3J6M2B4S1 (API v3) VID:PID 0483:374F
Info : using stlink api v3
Info : Target voltage: 3.234990
Info : clock speed 8000 kHz
Info : SRST line released
Info : stlink_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : STM32MP151CAAx.cpu0: hardware has 6 breakpoints, 4 watchpoints
Error: Could not find MEM-AP to control the core
Info : Listening on port 3334 for gdb connections
Info : Listening on port 3333 for gdb connections
ap 0 selected, csw 0x10006000
Info : accepting 'gdb' connection on tcp/3333
Error: Target not examined yet
Info : New GDB Connection: 1, Target STM32MP151CAAx.cpu2, state: unknown
undefined debug reason 7 - target needs reset
Error: Target not examined yet
Error: Target not examined yet
Error: Target not examined yet
Error: Target not examined yet
<< Execution Message >>
root@stm32mp1-fiscal:~# echo start > /sys/class/remoteproc/remoteproc0/state
[ 489.401238] remoteproc remoteproc0: powering up m4
[ 489.404634] remoteproc remoteproc0: loading /lib/firmware/updates/4.19.94/OpenAMP_TTY_echo_CM4.elf failed with error -20
[ 489.418946] remoteproc remoteproc0: loading /lib/firmware/updates/OpenAMP_TTY_echo_CM4.elf failed with error -20
[ 489.429594] remoteproc remoteproc0: loading /lib/firmware/4.19.94/OpenAMP_TTY_echo_CM4.elf failed with error -20
[ 489.440258] remoteproc remoteproc0: loading /lib/firmware/OpenAMP_TTY_echo_CM4.elf failed with error -20
[ 489.450382] remoteproc remoteproc0: Direct firmware load for OpenAMP_TTY_echo_CM4.elf failed with error -20
[ 489.460633] remoteproc remoteproc0: request_firmware failed: -20
[ 489.467095] remoteproc remoteproc0: Boot failed: -20
Regards
machilus
2020-04-06 5:49 AM
Hi @Machilus
I can not figure out why remote proc browse so many folders ?
What is the structure of the /lib/firmware on your target ?
Where /lib/firmware/updates/4.19.94/ come from ?
Where is the OpenAMP_TTY_echo_CM4.elf exactly before you start the firmware ?
If I got it right it's working with "st-image-weston". Can you share the succeeded trace of firmware start ?
Any difference in /lib/firmware folder structure ?
Hope it help,
Olivier
2020-04-06 6:46 PM
Hi @OlivierG (ST Employee)
I solved this problem.
In "st-image-core", "/lib/firmware" is a file.
In "st-image-weston", "/lib/firmware" is a directory.
In "st-image-core," I solved the problem by making "/lib/firmware" a directory.
Naturally, firmware exists within the "/lib/firmware" directory.
Thank you for helping me solve the problem.
Best regards.
Machilus.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.