2020-09-02 10:38 PM
I want to use remoteproc to load and start firmware on Coretex-M4 from Cortex-A7.
I refer to the following Wiki page.
https://wiki.st.com/stm32mpu/wiki/Linux_remoteproc_framework_overview
In above Wiki page, I have tried [4.1.1 Remote processor boot through sysfs].
However, I can't find "remoteprocX(e.g. remoteproc0)" directory in "/sys/class/remoteproc/" directory.
("/sys/class/remoteproc/" directory has no any sub-directory or files at all)
What should I do to create "remoteprocX(e.g. remoteproc0)" directory in "/sys/class/remoteproc/" directory?
Do I have to modify Linux kernel configuration or Device Tree?
For the reference, [Support for Remote Processor subsystem] and [STM32 remoteproc support] is enabled in Linux kernel configuration as modules , and these have being loaded by "modprobe" command.
Best regards.
H. Masuda
Solved! Go to Solution.
2020-10-15 1:05 AM
Hi @HMasu.1 ,
So, you need to have at least <&vdev0vring1> and <&vdev0buffer> in « memory-region » property, otherwise, it will not work as expected.
In case of non functionnal feature, I would recommand to look into one of the ST reference board device tree (example of m4_rproc entry in stm32mp15xx-dkx.dtsi) in order to cross-check that everything in fine in your own DT.
BR,
Christophe
2020-09-03 3:54 AM
Hi @HMasu.1,
Are you using the starter package image or a custom image ? If it is a custom image, could you list me what you added or removed from the default one ?
Best regards,
Armand
2020-09-04 1:41 AM
2020-09-08 6:57 AM
Hi @HMasu.1 ,
Actually functions related to remoteproc in the device tree don't seem to be different as the one in the starter package...
By the way, can you check in your kernel configuration if CONFIG_STM32_IPCC is enabled ? Remoteproc needs it to access its mailbox.
Else, it is probably due to when you probe the modules, may I ask you to send a screenshot of modprobe traces ?
Best regards,
Armand
2020-09-08 9:21 PM
2020-09-09 3:27 AM
Hi @HMasu.1 ,
It seems that you cannot enable CONFIG_STM32_IPCC by using modprobe, can you try to enable it via menuconfig ? (put a * instad of "M").
I got the same error as you if I modprobe it.
Best regards,
Armand
2020-09-10 12:45 AM
Hi @ArmandG ,
Thank you for your reply.
I enabled CONFIG_STM32_IPCC via menuconfig (put a * instad of "M").
However, the same error occurs, I can't find "remoteprocX(e.g. remoteproc0)" directory in "/sys/class/remoteproc/" directory.
Is there any other way to find out the cause?
Best Regards,
H. Masuda
2020-09-10 1:52 AM
Hello @HMasu.1 ,
You should try to put also "Support for remote processor subsystem" as built-in (the 4 lines with *) in order to start from scratch and see if you still have this problem.
If you don't, the problem may be due to the sequencing of modules, so try to module it one by one after.
If you still have the problem we need to look further in the device tree.
Best regards,
Armand
2020-09-10 8:54 PM
Hi @ArmandG ,
I have put "Support for remote processor subsystem" as built-in (the 4 lines with *), however, the same error occurs, I can't find "remoteprocX(e.g. remoteproc0)" directory in "/sys/class/remoteproc/" directory.
And, I have tried to module it one by one after, but I could only module "STM32 remoteproc support".
("Remoteproc System Resource Manager core" and "Remoteproc System Resource Manager device" could not be moduled Individually.)
In this configuration, the same error also occurs, I can't find "remoteprocX(e.g. remoteproc0)" directory in "/sys/class/remoteproc/" directory.
Should I investigate the differences between device trees in more detail?
Or is there another possible cause?
Best Regards,
H. Masuda
2020-09-11 7:12 AM
Hi @HMasu.1 ,
Can you send me the kernel trace, the .config generated by menuconfig and the .dtb ?
I will try to reproduce with your set up.
Best regards,
Armand
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.