STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Trouble creating v2.0.0 bootable SD card with create_sdcard_from_flashlayout.sh. Is there a pre-built sdcard.img file available?

Following the instructions found in en.FLASH-stm32mp1-openstlinux-5-4-dunfell-mp1-20-06-24.tar.xz and using create_sdcard_from_flashlayout.sh to write the data to an SD card did not work for me. When I inserted the card on the stm32mp157c-dk2 dev bo...

BMaha.1 by Associate II
  • 3863 Views
  • 4 replies
  • 0 kudos

Resolved! Starting M4 from BootRom

Is there a way to directly start M4 and run M4 firmware from BootRom.I am aware of the Engineering mode, however it requires the help of a debugger to copy the M4 firmware into the memory and run it. I like to do the same but in stand alone mode.I am...

Resolved! STM32MP1: OpenOCD cannot halt all cores

I am currently working on a design based around the STM32MP157C (mounted in the Seeed SoM - STM32MP157C).I am trying to connect to the M4 Core on the target but I cannot halt it. When I attempt to do it, the debugger can halt the A7 CPU0 but fails at...

bfh_dls by Associate II
  • 4601 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.