STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP157 UART RX suspend wakeup

We are having issues with STM32MP157 UART7 (address 40018000) exiting low power CStop mode and waking up Linux (v4.19 from ST github).We have confirmed that CStop mode is entered, and it can be exited using an external interrupt (55 pmic_irq), howeve...

drew by Associate III
  • 3477 Views
  • 3 replies
  • 0 kudos

Resolved! Error: fsbl1 (0x4): invalid address 0x4400 (min=0x80000) during loading flash_layout image to custom STM32MP1 board

Hi!During loading flash_layout image to custom STM32MP1 I've got following error after staring u-boot and truing to load information to partition 0x04 fsbl1:U-Boot 2020.01-stm32mp-r1 (Jan 06 2020 - 20:56:31 +0000)CPU: STM32MP157DAB Rev.ZModel: STMicr...

ASkri.1 by Senior
  • 3119 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.