2021-05-04 11:10 PM
Hi!
During loading flash_layout image to custom STM32MP1 I've got following error after staring u-boot and truing to load information to partition 0x04 fsbl1:
U-Boot 2020.01-stm32mp-r1 (Jan 06 2020 - 20:56:31 +0000)
CPU: STM32MP157DAB Rev.Z
Model: STMicroelectronics STM32MP157A-DK1 STM32CubeMX board
Board: stm32mp1 in trusted mode (st,stm32mp157a-stm32mp151-dk1-mx)
DRAM: 512 MiB
Clocks:
- MPU : 650 MHz
- MCU : 208.878 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
Fastboot key pressed, STM32Programmer key pressed, entering download mode...
WDT: Started with servicing (32s timeout)
NAND: 0 MiB
MMC: STM32 SD/MMC: 0
In: serial
Out: serial
Err: serial
invalid MAC address in OTP 00:00:00:00:00:00
stm32 vrefbuf timed out: -110
adc@0: can't enable vdd-supply!board_check_usb_power: single shot failed for adc@0[18]!
Net: No ethernet found.
Hit any key to stop autoboot: 0
Boot over usb0!
Error: fsbl1 (0x4): invalid address 0x4400 (min=0x80000)
DFU alt info setting: done
crq->brequest:0x0
Reset requested
#
UPLOAD ... done
flash-layout .tsv file:
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl1-boot Binary none 0x0 ../../arm-trusted-firmware/tf-a-stm32mp157a-stm32mp151-dk1-mx-serialboot.stm32
- 0x03 ssbl-boot Binary none 0x0 ../../bootloader/u-boot-stm32mp157a-stm32mp151-dk1-mx-trusted.stm32
P 0x04 fsbl1 Binary mmc0 0x00004400 ../../arm-trusted-firmware/tf-a-stm32mp157a-stm32mp151-dk1-mx-trusted.stm32
P 0x05 fsbl2 Binary mmc0 0x00044400 ../../arm-trusted-firmware/tf-a-stm32mp157a-stm32mp151-dk1-mx-trusted.stm32
PD 0x06 ssbl Binary mmc0 0x00084400 ../../bootloader/u-boot-stm32mp157a-stm32mp151-dk1-mx-trusted.stm32
P 0x21 boot System mmc0 0x00284400 ../../st-image-bootfs-openstlinux-weston-stm32mp1-disco-mx.ext4
P 0x22 vendorfs FileSystem mmc0 0x04284400 ../../st-image-vendorfs-openstlinux-weston-stm32mp1-disco-mx.ext4
P 0x23 rootfs FileSystem mmc0 0x05284400 ../../st-image-weston-openstlinux-weston-stm32mp1-disco-mx.ext4
P 0x24 userfs FileSystem mmc0 0x33C84400 ../../st-image-userfs-openstlinux-weston-stm32mp1-disco-mx.ext4
Custom board have mmc connected to SDMMC0 interface and pmic connected to i2c2 instead of i2c4. And nothing more.
I've no ideas which way to go...
Could you please suggest me a ways to debug such situation.
Thank you in advance
Looking forward for your reply
Solved! Go to Solution.
2021-05-12 10:31 PM
Answering myself... SD and MMC requires different flash-layouts.
2021-05-12 10:31 PM
Answering myself... SD and MMC requires different flash-layouts.
2021-05-14 5:06 AM
to complete : each MMC partition needs to be aligned on MMC erase block
https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#GPT_partition_sizes
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.