STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! [Solved] Problem tring to run gtk hello world (developper package) with bitbake (distribution package) : don't find how to properly source gtk.

Hello,I'm trying to embed an app in the st-linux distribution. I mean that the goal is to have it compiled with bitbake and integrated in a custom st-image-weston.I tried to use the gtk hello world example of Developper section (that run without prob...

BJola.1 by Associate II
  • 7046 Views
  • 5 replies
  • 0 kudos

SPI Read in uboot - SPI2

Hi ,Actally i want to read a PISO shifht register as spi slave.Device Tree: spi2_pins_a: spi2-0 {  pins1 { pinmux = <STM32_PINMUX('A', 9, GPIO)>, /* uart8_tx */ <STM32_PINMUX('I', 2, GPIO)>, /* uart8_tx */ <STM32_PINMUX(...

Ganesh.T by Associate II
  • 1624 Views
  • 1 replies
  • 0 kudos

Good afternoon, Olivier. Thanks for the help. But I saw a problem with MPU Serial (COM3). I ran ipconfig in Linux and found the real address of usb0 192.168.7.2.

Good afternoon, Olivier. Thanks for the help. But I saw a problem with MPU Serial (COM3). I ran ipconfig in Linux and found the real address of usb0 192.168.7.2 after that, the console worked.But the board does not allow debugging. I must have done s...

Vlaty.1 by Senior
  • 1146 Views
  • 0 replies
  • 0 kudos

Resolved! M4 Core ITM trace

Hi,Looking at the reference manual, en.DM00327659.pdf, page 3929 it seems the simple way of debugging previous M4 processors using printf() redirect to the ITM and then using the SWO pin/STLINK interface could be used on the MP1 M4 core as well.But t...

K.Ata15 by Associate III
  • 3775 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.