STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! [Solved] Why bitbake st-image-weston don't generate .dts files and how to force it ?

I'm trying to edit the device tree of the distribution but there is no .dts or .dtsi files in all the distribution package directories. The only way I found to experiment modifying the device tree is doing it with developper package (I modified stm32...

BJola.1 by Associate II
  • 4905 Views
  • 6 replies
  • 0 kudos

Resolved! My STM32MP157F-DK2 is powered by 5V 3A PSU. but at the boot up time, always it displays the warning

My STM32MP157F-DK2 is powered by 5V 3A PSU. but at the boot up time, always it displays the warning *****************************************************    WARNING 500mA power supply detected    **   Current too low, use a 3A power supply!   *******...

Resolved! facing ERROR: icu-66.1-r0 do_compile: oe_runmake failed during Building the OpenSTLinux distribution

Hi,I'm working on STM32MP157A-DK1. By following this linkhttps://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package tried building the image for STM32MP157A-DK1 but i facing the error ERROR: icu-66.1-r0 do_compile: oe_runmake failed during build...

Arahm.1 by Associate II
  • 7002 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.