STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How do we write read and erase the QSPI memory(NOR flash) in Stm32mp157a Uboot?

Hi,We are using Stm32mp157a processor and uboot2018.11 version.We have QSPI interface to NOR flash. We want to write,Read and erase the Data in Qspi Memory(i.e,Nor flash).We want to boot the image from Nor flash,How can we do that ?Thanks in Advance.

Resolved! Regarding STM32mp157A UART in U BOOT

Hi,We are using stm32mp157a processor and we are working on uboot-v2018.11 at Linux side. I have an idea on board-debug-uart_init().Path for board_debug_uart_init().Path :board/st/stm32mp1/board.cIn board-debug-uart_init() .We have only UART_TX infor...

在根�?�ST�??供的tf-a编译阶段,为什么我使用make -f Makefile.sdk TF_A_CONFIG=trusted TFA_DEVICETREE=stm32mp157c-dk2 all这个指令编译的时候会报下�?�这些错误?

在根�?�ST�??供的tf-a编译阶段,为什么我使用make -f Makefile.sdk TF_A_CONFIG=trusted TFA_DEVICETREE=stm32mp157c-dk2 all这个指令编译的时候会报下�?�这些错误?

Ffu.1 by Associate II
  • 7786 Views
  • 7 replies
  • 0 kudos

Resolved! Can someone please help. We are trying to implement a KSZ8041FTL Ethernet PHY using an STM32MP157C. We are not able to connect to the device via MDIO. The device does not respond.

We are trying to implement a KSZ8041FTL in an embedded design. We are using an STM32MP157 device in a SOC provided by Octavo systems (OSD32MP157C-512M-BAA). We have used design resources provided by Microchip and followed examples provided. We have f...

PZak.1 by Associate III
  • 26162 Views
  • 18 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.