2021-10-25 6:29 AM
Hello, my main seriale console should be USART2 instead of UART4. I modified the kernel dts as follows:
chosen {
stdout-path = "serial0:115200n8";
};
aliases {
ethernet0 = ðernet0;
mmc0 = &sdmmc1;
mmc1 = &sdmmc2;
serial0 = &usart2;
};and it configures correctly the kernel console.
If I try the same modification in tf-a and u-boot dts, at boot i see the log starting on uart4, but it blocks at this point
Preparing exit to normal world
No serial driver foundShould I modify some boot env too?
Solved! Go to Solution.
2021-11-12 4:52 AM
Hi,
For the uboot project , I added CONFIG_DEBUG_UART_BASE=0x4000E000 (usart2 base address) in the defconfig, I added
chosen {
stdout-path = "serial0:115200n8";
};
aliases {
ethernet0 = ðernet0;
mmc0 = &sdmmc1;
mmc1 = &sdmmc2;
serial0 = &usart2;
serial1 = &uart4;
};
&pinctrl {
usart2_pins_d: usart2-2 {
pins1 {
pinmux = <STM32_PINMUX('D', 5, AF7)>; /* USART2_TX */
bias-disable;
drive-push-pull;
slew-rate = <3>;
};
pins2 {
pinmux = <STM32_PINMUX('D', 6, AF7)>; /* USART2_RX */
bias-disable;
bias-pull-up;
};
};
usart2_idle_pins_d: usart2-idle-2 {
pins1 {
pinmux = <STM32_PINMUX('D', 5, ANALOG)>; /* USART2_TX */
};
pins2 {
pinmux = <STM32_PINMUX('D', 6, AF7)>; /* USART2_RX */
bias-disable;
};
};
usart2_sleep_pins_d: usart2-sleep-2 {
pins {
pinmux = <STM32_PINMUX('D', 5, ANALOG)>, /* USART2_TX */
<STM32_PINMUX('D', 6, ANALOG)>; /* USART2_RX */
};
};
};
&usart2 {
pinctrl-names = "default", "sleep", "idle";
pinctrl-0 = <&usart2_pins_d>;
pinctrl-1 = <&usart2_sleep_pins_d>;
pinctrl-2 = <&usart2_idle_pins_d>;
status = "okay";
};
in the .dts.
I added this part also in the dts of the tf-a project.
Then i generated the fip bianary file. When flashing, I see cubeprogrammer Logs on usart2.
2021-10-25 9:39 AM
Hi @Lmoio.1 ,
You do not only need to change serial0 from uart4 to usart2. You have also to be sure that usart2 is defined in the DT (Device Tree) and is enabled:
status = "okay";and that the pins are configured.
Please verify in the tf-a and u-boot dts that it is the case
Regards,
Kevin
2021-10-26 12:30 AM
yes, i added
&pinctrl {
m4_adc12_pins_a: m4-adc12-pins-0 {
pins {
pinmux = <STM32_PINMUX('F', 13, RSVD)>, /* ADC2 in2 */
<STM32_PINMUX('A', 6, RSVD)>,/* ADC2 in3 */
<STM32_PINMUX('F', 14, RSVD)>, /* ADC2 in6 */
<STM32_PINMUX('C', 0, RSVD)>; /* ADC12 in10 */
};
};
usart2_pins_d: usart2-2 {
pins1 {
pinmux = <STM32_PINMUX('D', 5, AF7)>; /* USART2_TX */
bias-disable;
drive-push-pull;
slew-rate = <3>;
};
pins2 {
pinmux = <STM32_PINMUX('D', 6, AF7)>; /* USART2_RX */
bias-disable;
};
};
usart2_idle_pins_d: usart2-idle-2 {
pins1 {
pinmux = <STM32_PINMUX('D', 5, ANALOG)>; /* USART2_TX */
};
pins2 {
pinmux = <STM32_PINMUX('D', 6, AF7)>; /* USART2_RX */
bias-disable;
};
};
usart2_sleep_pins_d: usart2-sleep-2 {
pins {
pinmux = <STM32_PINMUX('D', 5, ANALOG)>, /* USART2_TX */
<STM32_PINMUX('D', 6, ANALOG)>; /* USART2_RX */
};
};
};
&uart4 {
status = "disabled";
};
&usart2 {
pinctrl-names = "default", "sleep", "idle";
pinctrl-0 = <&usart2_pins_d>;
pinctrl-1 = <&usart2_sleep_pins_d>;
pinctrl-2 = <&usart2_idle_pins_d>;
status = "okay";
};but it still starts on uart4 and prints "no serial driver found" when launching uboot.
Should I modify CONFIG_DEBUG_UART_BASE= in the .config file?
2021-10-26 2:09 AM
Hi @Lmoio.1 ,
I do not think this error is due to CONFIG_DEBUG_UART_BASE.
Please can you send me:
To check if I find an error.
Regards,
Kevin
2021-10-26 8:25 AM
2021-10-26 8:25 AM
2021-10-26 8:29 AM
Another question, I noticed that if I don't connect a TTL cable to the uart4 that i'm trying to use, kernel does not start, whereas if i connect a cable (it can also be not connected to a pc) the kernel starts. Should I remove from the u-boot defconfig CONFIG_REQUIRE_SERIAL_CONSOLE option?
2021-10-26 9:17 AM
Hello @Lmoio.1 ,
You forgot in the tf-a dts to add the USART2 in etzpc node. Please can you add this line in etzpc node:
DECPROT(STM32MP1_ETZPC_USART2_ID, DECPROT_NS_RW, DECPROT_UNLOCK)As explained in the wiki https://wiki.st.com/stm32mpu/wiki/ETZPC_device_tree_configuration#DT_bindings_documentation
The ETZPC binding assigns the peripheral to the desired CORE, so in your case, you must specify the USART2 and assign it to the non secure linux.
Hope it helps,
Kevin
2021-10-27 12:55 AM
I added your suggestion, but STprogrammer fails at downloading because it cannot reconnect to the device.
09:50:40 : Time elapsed during download operation: 00:00:01.194
09:50:40 : RUNNING Program ...
09:50:40 : PartID: :0x03
09:50:40 : Reconnecting the device ...
09:51:10 : Error: Unable to reconnect the target device: time out expired
09:51:10 : Error: Start operation failed at partition 0x03
09:51:10 : Error: TSV flashing service failed
09:51:10 : Warning: Connection to device 0x500 is lost
09:51:10 : Disconnected from device.
2021-10-28 1:42 AM
hello @Lmoio.1 ,
Did you have some logs on your usart2? Maybe your TF-A or u-boot is crashing and prevent the flashing operation.
If you have logs can you send them please.
And then can you run the STM32CubeProgrammer from the console and please share with me the log too:
https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer#How_to_flash_with_STM32CubeProgrammer
You have to run the STM32_Programmer_CLI:
STM32_Programmer_CLI -c port=<DEVICE_PORT_LOCATION> -w [<file.tsv>]Regards,
Kevin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.