2021-12-23 6:37 AM
Hi,
I'm using stm32mp157a-dk1 and I would like to use rpmsg_sdb for exchanging data buffers with the coprocessor (https://wiki.st.com/stm32mpu/wiki/How_to_exchange_data_buffers_with_the_coprocessor).
I built the image for the A7 following the "STM32MP1 Distribution Package" tutorial without problem (https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package#Flashing_the_built_image).
But in the dev folder I can't find the rpmsg_sdb device.
Is there a prebuild image for A7 with this driver?
If not, how can I add the recipe rpsmg-sdb-mod Yocto recipe to the image of the distribution tutorial using bitbake?
In case, is there other ways to get the device rpmsg_sdb?
Thank you in advance.
Best regards,
Andrea Segalla
Solved! Go to Solution.
2021-12-23 7:08 AM
Hi @ASega.1 ,
The device rpmsg_sdb is populated thanks to recipes in :
Refer to the readme in order to have the complete instruction to integrate it in your build
Olivier
2021-12-23 7:08 AM
Hi @ASega.1 ,
The device rpmsg_sdb is populated thanks to recipes in :
Refer to the readme in order to have the complete instruction to integrate it in your build
Olivier
2021-12-24 4:06 AM
Dear @Community member ,
Thanks for the reply.
I tried this morning to add the layer meta-st-stm32mpu-app-logicanalyser following the tutorial you suggest to me but it returns me errors in the last command:
bitbake-layers add-layer ../layers/meta-st/meta-st-stm32mpu-app-logicanalyser
the errors returned:
NOTE: Starting bitbake server...
Traceback (most recent call last):
File "/home/midac/ProjectYocto/sdb/openstlinux-5.10-dunfell-mp1-21-11-17/layers/openembedded-core/bitbake/bin/bitbake-layers", line 95, in <module>
ret = main()
File "/home/midac/ProjectYocto/sdb/openstlinux-5.10-dunfell-mp1-21-11-17/layers/openembedded-core/bitbake/bin/bitbake-layers", line 63, in main
tinfoil.prepare(True)
File "/home/midac/ProjectYocto/sdb/openstlinux-5.10-dunfell-mp1-21-11-17/layers/openembedded-core/bitbake/lib/bb/tinfoil.py", line 414, in prepare
self.run_command('parseConfiguration')
File "/home/midac/ProjectYocto/sdb/openstlinux-5.10-dunfell-mp1-21-11-17/layers/openembedded-core/bitbake/lib/bb/tinfoil.py", line 470, in run_command
raise TinfoilCommandFailed(result[1])
bb.tinfoil.TinfoilCommandFailed: Traceback (most recent call last):
File "/home/midac/ProjectYocto/sdb/openstlinux-5.10-dunfell-mp1-21-11-17/layers/openembedded-core/bitbake/lib/bb/command.py", line 74, in runCommand
result = command_method(self, commandline)
File "/home/midac/ProjectYocto/sdb/openstlinux-5.10-dunfell-mp1-21-11-17/layers/openembedded-core/bitbake/lib/bb/command.py", line 275, in parseConfiguration
command.cooker.parseConfiguration()
File "/home/midac/ProjectYocto/sdb/openstlinux-5.10-dunfell-mp1-21-11-17/layers/openembedded-core/bitbake/lib/bb/cooker.py", line 433, in parseConfiguration
self.handleCollections(self.data.getVar("BBFILE_COLLECTIONS"))
File "/home/midac/ProjectYocto/sdb/openstlinux-5.10-dunfell-mp1-21-11-17/layers/openembedded-core/bitbake/lib/bb/cooker.py", line 1225, in handleCollections
raise CollectionError("Errors during parsing layer configuration")
bb.cooker.CollectionError: Errors during parsing layer configuration
Do you have the same problem or probably I made some mistake?
Thanks in advance.
Best Regards,
Andrea
2022-01-03 8:49 AM
Hi @ASega.1 ,
The add-layer steps works properly at my end.
Double check all the procedure and eventually retry on a clean environment.
Olivier
2022-01-05 4:22 AM
Hi @Community member ;
I tried again and now it works.
Thanks so much for the helping.
Best Regards,
Andrea
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.