STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP157C with MII PHY not working

I am using a KSZ9021GN PHY in MII mode. Due to supply chain issues we had to resort to this PHY. (Cube MX says I can't use GMII mode). I am experiencing this apparently common issue: [ 15.650981] dwmac4_dma_reset err [ 15.652849] stm32-dwmac 580...

BillR by Senior
  • 3955 Views
  • 3 replies
  • 0 kudos

Resolved! Dear Experts, can I use the DCMI on the STM32MP15x, with the Cortex M4, for an asyncron connected non-camera source?

I have to design a system, where a STM32MP157, with its embedded Cortex M4, communicate with other clients over a high-speed serial connection. There should be a 10 : 1 serializer for the MOSI line, and a 1 : 10 deserializer for the MISO line (from t...

Resolved! Why do I get inaccurate values on my analog to digital converter on my STM32MP1?

I've just watched a few tutorials on ADC, and I've enabled IN1 on ADC1 which seems to map to the connector labeled A3 as per this doc.I then added the following to my main.c within the CM4 project.uint32_t raw = 0; char msg[100]; HAL_ADC_Start(&hadc1...

msche.1 by Associate III
  • 6076 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.