STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! android on stm32mp157c-dk2

Hi Nicolas L (ST Employee),I have read the past article that you provide sources and directives to allow building the Android 10 delivery for the STM32MP157C-DK2.Could you please send me the solution?I hope you will be able to reply to me.By the way,...

HiroM by Associate II
  • 3117 Views
  • 4 replies
  • 0 kudos

i2c2

I'm working with the DevBoard from Myir MYD-YA-157C which has the stm32mp157 MPU. I'm trying to chech the i2c from the M4 in the Engineering mode and have a problem.When I tied the I2C_TwoBoards_ComIT, it works. At least it generates the I2C5_ER_IRQ....

How do I fix "undefined reference to `OPENAMP_create_endpoint'" within the OpenAmp source.

I've added OPENAMP through the middleware after enableing the IPCC interrupts, but now I'm getting the following error and an error in the actual OPENAMP source that's included!/opt/st/stm32cubeide_1.8.0/plugins/com.st.stm32cube.ide.mcu.externaltools...

msche.1 by Associate III
  • 2060 Views
  • 1 replies
  • 0 kudos

Resolved! Time of erase after a tamper

Hi all,I am using MPU ref. STM32MP153F, do you say me what is the time that elapsed between a tamper is detected and the backup resister are finishing erased?And the backup SRAM?Thank you in advance

FAlca.1 by Associate II
  • 1864 Views
  • 1 replies
  • 0 kudos

Resolved! STM32MP157 Errata 2.3.8, "eMMC boot Timeout too short", causes problems with available eMMCs.

The STM32MP157 demands a maximum time of 10 ms from reset command to boot partition data. According to JEDEC No 84-B51 the maximum time from reset command to the first data is up to 1 second (tBD):All data sheets of eMMCs that I found specify their b...

0693W00000KcGd5QAF.png
SigiBue by Associate
  • 2406 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.