2022-03-09 11:45 PM
Hi everyone!
I want to use a hardware semaphore to access SRAM4 memory from both Linux and M4 firmware on STM32MP157A-DK1 board. There are no problems with the M4 firmware. But for Linux I have to create a driver. There is an example in this article: https://wiki.st.com/stm32mpu/wiki/Hardware_spinlock_overview
But according to this example, I can't choose the number of the hardware semaphore that I want to use. I ask for advice on how best to organize what I want to do. Maybe I can use a hardware semaphore from user space?
2022-03-11 8:56 AM
Hello @AlexandrShipovsky
The semaphore number is selected thanks to the device tree configuration as described here:
https://wiki.st.com/stm32mpu/wiki/HSEM_device_tree_configuration#DT_configuration_examples
2022-03-15 5:46 AM
Okay, thank you for answer. But I found another way. In the driver code I write this:
hwlock = hwspin_lock_request_specific(HSEM_ID);
if (hwlock)
{
/* try to take it, but don't spin on it */
ret = hwspin_trylock(hwlock);
if (!ret) {
pr_info("lock is taken\n");
}
/*
* we took the lock, do our thing now, but do NOT sleep
*/
hwspin_unlock(hwlock);
}It work for any number hardware semaphore
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.