STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I have an STM32MP157F-DK2 and am attempting to create a build using Yocto. I am using meta layers poky, openembedded, and st-stm32mp. I can build core-image-minimal. This build lacks WiFi and USB OTG which are needed.

The image that comes with the board has WiFI and USB OTG working. I am adding additional networking (VPN, firewall) to my Yocto build. I have attempted to build core-image-base and am able to see the wlan0 adapter but something in that build is disab...

KBarr.1 by Associate
  • 1110 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.