How to connect the stm32mpu157f-dk2 and the amicam1?
@Alain FERRARI
Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.
@Alain FERRARI
Hy there!I'm new on ST platforms and development environments (I'm used to Netbeans-like ones).Well, I would like to copy (automatically) both .elf executable and the .map files in given folder after building the projet.This folder ("Out") is placed ...
Hplip is only 3.19.12, and there is no higher version.
My package is http://packages.openstlinux.st.com/3.1 ,I cannot update cups.When I install cups,the "cups : Depends: libdbus-1-3 (>= 1.12.20) but 1.12.16-r0.1 is to be installed" appeared,How can I install the libdbus-1-3 (>= 1.12.20) ? Thanks.
I want to store some configurations in the OTP. The datasheet states that the OTP word 59 to 95 are free for users. In DK boards, OTP word 59 is already claimed as board_id, so I use word 60 as my starting point. Currently, I am using both environmen...
Hi! It's my understanding that ST are moving a lot of work for power management and clocking out of ATF and to OP-TEE. In preparation for this shift my co-developer and I have started out trying to build and run the following software on the STM32MP1...
I have acquired both boards. Here is the link to the video:https://www.youtube.com/watch?v=FSIYaWOmzS4
Hello,When I plugged the IMX477 on a USB port and I have the following msg:[ 7307.355686] usb 2-1.3: new high-speed USB device number 5 using ehci-platform[ 7307.519593] uvcvideo: Found UVC 1.00 device Arducam IMX477 HQ Camera (0c45:636d)[ 7307.53462...
Hi everyone, I recently picked up a STM32MP157F-DK2 board and trying out this embedded linux. Very new to it all.I did some research and it looks like the traditional way is to use one of the build systems, such as buildroot to create your own distri...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.