STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Can't get out of DFU mode.

Hello,Using a custom board loosely based on STM32mp157F-DK2we are using boot0 and boot2 pins.According to documentation,boot mode configuration is as follows;Boot Mode     BOOT2  BOOT0Recov/DFU        0      0Nor              0      1Reser...

Resolved! how to use jtag in stm32mp157f-dk2

stm32mp157f-dk2 is not embedded jtag connector,but i want to use jtag debugger.​st-link(stm32f103cbt6) embedded in stm32mp157f-dk2 has jtag pin(T_JTCK, T_NRST, T_SWO, T_JTMS)Q1. Can't I use jtag with only ST-LINK USB CONNECTOR (5 pin)?Q2. what should...

0693W00000bhLyaQAE.png
SKim.36 by Associate II
  • 4509 Views
  • 5 replies
  • 0 kudos

Good afternoon! I'm trying to use TSC2046 based touchscreen device on a STM32MP157C-DK2 based custom board. I get SPI transfer time-out when touching the screen. Does anyone have a similar problem ?

I'm using spi5 and my device tree settings are &spi5 { pinctrl-names = "default", "sleep"; pinctrl-0 = <&spi5_pins_a>; pinctrl-1 = <&spi5_sleep_pins_a>;    #address-cells = <1>;    #size-cells = <0>; num-cs = <1>; is-decoded-cs = <0>; cs-gpios = <&gp...

Ronte.1 by Associate III
  • 3960 Views
  • 4 replies
  • 0 kudos

How to enable PWR_USB_SW in STPMIC?

Hello,I am working on a custom board based on stm32mp157 and I have the need to enable the PWR_USB_SW through the ST PMIC. So far, I identified the bit VBUSOTG_ON in register BST_SW_CR (0x40) but I had no success in configuring it via devicetree or v...

bimorqt by Associate III
  • 5703 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.