2023-03-22 6:34 AM
Hello,
I want to upgrade my hardware to new openstlinux kirkstone release november 2022.
First test on eval board was successful.
I have written custom device tree files and compiling for tf-a, u-boot, fip and kernel is fine.
However when I try to flash my image flashlayout to my custom board I get a "ERROR: Illegal access to 0xfffffff0:"
See following for complete output:
NOTICE: CPU: STM32MP157C?? Rev.Z
NOTICE: Model: OSD32MP1 epis shuttle sps board
INFO: PMIC version = 0x21
INFO: Reset reason (0x214):
INFO: IWDG2 Reset (rst_iwdg2)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.6-stm32mp1-r2.0(debug):v2.6-dirty(a1f02f4f)
NOTICE: BL2: Built : 13:14:26, Nov 23 2021
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000Khz
INFO: Memory size = 0x20000000 (512 MB)
INFO: DFU USB START...
INFO: phase ID :3, Manifestation 3 at c7110ac2
INFO: Send detach request
INFO: Receive DFU Detach
INFO: DFU USB STOP...
INFO: BL2: Loading image id 1
INFO: Loading image id=1 at address 0x2ffff000
INFO: Image id=1 loaded: 0x2ffff000 - 0x2ffff226
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2ffc5000
INFO: Image id=4 loaded: 0x2ffc5000 - 0x2ffd9820
INFO: BL2: Skip loading image id 8
INFO: BL2: Skip loading image id 9
INFO: BL2: Loading image id 2
INFO: Loading image id=2 at address 0xc0500000
INFO: Image id=2 loaded: 0xc0500000 - 0xc05140a8
INFO: BL2: Loading image id 16
INFO: Loading image id=16 at address 0x2ffc0000
INFO: Image id=16 loaded: 0x2ffc0000 - 0x2ffc39a0
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: Image id=5 loaded: 0xc0100000 - 0xc01e4534
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0x2ffc5000
INFO: SPSR = 0x1d3
NOTICE: SP_MIN: v2.6-stm32mp1-r2.0(debug):v2.6-dirty(a1f02f4f)
NOTICE: SP_MIN: Built : 13:14:26, Nov 23 2021
INFO: ARM GICv2 driver initialized
INFO: Set calibration timer to 60 sec
INFO: stm32mp1 IWDG1 is secure
INFO: SP_MIN: Initializing runtime services
INFO: SP_MIN: Preparing exit to normal world
ERROR: Illegal access to 0xfffffff0:
ERROR: FAIL_ID = 0x4c0
ERROR: Non-Secure
ERROR: Privilege
ERROR: Read
PANIC at PC : 0x2ffc9739
Exception mode=0x00000016 at: 0x2ffc9739
What is wrong in my configuration or device tree?
Error messages come from tf-a, not sure if it is related to u-boot and fip.
Any suggestion is appreciated! Thanks!
Greez Dmn
2023-04-07 2:29 AM
Hi @DmnSd
Sorry to come late in this thread ?
Where do you stand with this issue ?
Did you find the issue ?
I read you are using OSD32MP1. Did you try to contact Octavo support ?
Did you migrate to kirkstone release from ST material or Octavo ones ?
Did your system works properly with previous version ?
Thanks
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.