STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

when i use STMCubeMX(version6.8.0) to generate the code about STM32MP157DAA1,i find whether i define the GPIO's user label,it just can't generate in the keil project.

i also find some people say this is a bug,repeatedly click the setting of user label can be solved,but i try it's can‘t figure it out.....By the way,GPT also not give the correct solution (this is why i am here)​this is my first question in this com...

GGree.2 by Associate II
  • 2768 Views
  • 4 replies
  • 0 kudos

Resolved! cube mx does not launch workspaces

Greetings,in the video STM32MP1 workshop - 9 OpenSTLinux BSP pin Muxing - STM32CubeMX lab after modifying the DK2_TIMER_A7 project in the mx cube directly open the project in workbench from generate code, open the file.On my pc this doesn't happen, t...

MMarc.11 by Associate II
  • 6719 Views
  • 4 replies
  • 0 kudos

Using sftp client on STM32MP1 Linux

I am having trouble how to setup the Linux system on the STM32MP1 so that I can use sftp to upload data gathered by the device to an external server.What happens is that once the connection is established it immediately closes again, so there is no t...

SFuch.1 by Associate III
  • 2408 Views
  • 1 replies
  • 0 kudos

Resolved! I'd like to output the PPS waveform on the STM32MP157D-EV1 board. But it's not outputting.

I found the pin of PG8 on the GPIO pin map on the board. So I connected to PG8 and GND to connect with oscilloscope.In the picture, the blue line is the oscilloscope's GND port.I connected the board and the oscilloscope like the picture above. And I ...

0693W00000aJSdSQAW.png 0693W00000aJSeGQAW.jpg 0693W00000aJSeaQAG.jpg
kKim.1 by Associate II
  • 1825 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.