2023-03-28 4:39 PM
Hello,
I'm writing to inquire if there is documentation/support for developing non-linux operating systems using the STM32 MPU discovery kits. So far I've only found Cube support and documentation for ST's custom linux distro. Obviously, a processor being a processor, it can run anything I put in the ROM. But I'd like to be able to utilize some of the development tools that these boards are supposed to support to make the development/debugging experience easier.
I'm using a STM32MP157D-DK1, in case that makes any major difference.
2023-04-03 5:46 AM
Hello @JAppe.1 ,
Unfortunately, the only OS that ST supports on MPU side is OpenSTLinux (which is our specific Linux distribution). You are right, there are various way to use and program a microprocessor, but ST specific Linux is the only one supported by our teams.
Kind regards,
Erwan.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.