2023-11-18 12:14 PM - edited 2023-11-18 12:16 PM
Hello,
I've tried measure period of GPS PPS which is very high accuracy. I'm using TIM5 input capture mode, reset slave mode. The TIM5 CCR1 gives value 208877646 that is wrong because I use high accurate generator for sys clock. The right value is about 209000000. So maybe anyone meet the problem?
Thanks,
Alex.
Solved! Go to Solution.
2023-11-20 12:36 AM
Hi @alex_vm ,
could you check the real TIM5 clock using :
grep -E "clock|tim5_k" /sys/kernel/debug/clk/clk_summary
in starter package, the clock is defined as 208877930Hz, so your results sound good with this value (tolerance of HSE oscillator).
Regards.
2023-11-20 12:36 AM
Hi @alex_vm ,
could you check the real TIM5 clock using :
grep -E "clock|tim5_k" /sys/kernel/debug/clk/clk_summary
in starter package, the clock is defined as 208877930Hz, so your results sound good with this value (tolerance of HSE oscillator).
Regards.
2023-11-20 7:44 AM - edited 2023-11-20 7:45 AM
Hi Patrick
Thank you for your help. I forget to write in the start topic I'm using M4 in standalone mode .But as I think the cause is a same.
BR
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.