STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Re: STM32MP1 FDCAN issues

I am setting up the fd-can protocol on stm32mp1, please let me know after creating the dts file from stm32mx , how to transfer that file to stm32mp1 to use, do I use the command root@stm32mp1:~# ls / sys/class/netend0 lo usb0 , it doesn't show that t...

Resolved! FDCAN can not start, no clock found

after follow the wiki, the can0(m_can2) can not start up on stm32mp157d-dk1root@stm32mp1:~# dmesg | grep can[ 0.384348] can: controller area network core[ 0.384666] can: raw protocol[ 0.384678] can: broadcast manager protocol[ 0.384695] can: netlink ...

Huibean by Associate II
  • 10742 Views
  • 9 replies
  • 0 kudos

Resolved! STM32MP151C SPI5 clock much slower

I am trying to configure SPI5 on STM32MP151C where MPU is a master and ESP32C6 is a slave. The clock used in the device tree is HSI 64MHz. SPI driver is running with 2MHz configured and divisor in the SPI_CFG1 register is correctly set to 32. In the ...

vsaakian by Associate III
  • 3674 Views
  • 2 replies
  • 1 kudos

STM32MP153 - How to enable HSI clock?

Hi, I set MCO1 using HSE clock and get 8MHz working well (my HSE is 8MHz)But I need 16MHz or higher on MCO1, so I changed to MCO1 source clock by HSI but there is nothing.I tested other CSI, HSE, ... MCO1 work, except for HSI.I think there is somethi...

Dat Tran by Senior II
  • 1700 Views
  • 1 replies
  • 0 kudos

Issue regarding DDR3

HelloI'm using stm32mp157aaa3 processor in our custom board.And I'm working on DDR3L with arm-trusted-firmware(V2.5) ddr3 routines as my reference code and reference manual(RM0436) and Application not(AN5168).When I am hard-coding the register values...

m4projects-stm32mp1-1.6.0 fetcher failure

Hi,I'm trying to build core-image-minimal yocto project for my STM32MP157D-DK1 board according to digikey tutorial and I stuck at fetching m4projects dependency. Does anybody faces and resolved this issue?My build conf:Build Configuration:BB_VERSION ...

dnj by Associate III
  • 1649 Views
  • 0 replies
  • 0 kudos

Resolved! TF-A hangs on stm32mp157d-dk1

Hello all, As part of the evaluation of the 32MP15 series, I was trying to build the u-boot and TF-A binaries. I tried the u-boot SPL bring up and it seems to be working fine (except for failure to launch the Linux Kernel, as per your late updates). ...

Resolved! STM32MP131FAF7T how to program PMIC

I have a custom built  STM32MP131FAF7T board and can't set my VOUT2. The only line that is down is my VDD DDR Lines since I can't program my PMIC (STPMIC1DPQR) to have the VOUT2 to be 1.35 volts instead of 1.1 volts. My VCPU is at 1.2V, VDD is at  3....

T_Dodd by Associate
  • 2069 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.