2024-11-03 1:27 AM
Hey there,
I have a custom stm32mp153c based board. I adapted bootloaders/optee/kernel from scarthgap branch of meta-st-stm32mp and have everything booting (tf-a 2.8, u-boot 2022.10, optee 3.19, kernel 6.1.28). The only remaining warnings I have are these:
root@stm32mp1:~# dmesg | grep pmic
[ 0.459590] stpmic1 2-0033: PMIC Chip Version: 0x21
[ 0.497690] stpmic1-regulator 5c009000.i2c:stpmic@33:regulators: Failed to create device link (0x180) with 2-0033
[ 0.506580] stpmic1-regulator 5c009000.i2c:stpmic@33:regulators: Failed to create device link (0x180) with 2-0033
[ 0.516882] stpmic1-regulator 5c009000.i2c:stpmic@33:regulators: Failed to create device link (0x180) with 2-0033
I found only two threads mentioning the issue, but couldn't figure out how to fix it and even got an impression that these are somehow expected?
Any hints where the warnings come from?
Thanks,
Vyacheslav
2024-11-04 1:24 AM
Hi @UVV
Scarthgap is not yet supported by OpenSTLinux (will come soon).
Wait few weeks or go back to Mickeldore: https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ecosystem_release_note#OpenSTLinux_for_Arm-C2-AE_Cortex-C2-AE-A
Regards.
2024-11-04 1:32 AM
Perhaps I was not clear with my statement, but I don't use scarthgap branch, I'm still on kirkstone. I only took the bootloader/kernel from the scarthgap branch. I see that kernel version mentioned in your link is newer though. I could give it a try.
As a yocto maintainer, I'm not sure I like your advise to use non LTS version, and why updates are provided in mickeldore rather than in LTS branch.
2024-11-04 2:13 AM
Hi,
I'm not SW expert, just try to find out rationale of your warning messages.
We provide a new ecosystem major release almost every year, but as Yocto LTS is every two years, we then have one intermediate release on a 'non-LTS' Yocto version.
If you want only LTS Yocto, as you do, you should stick to our latest Kirkstone release https://wiki.st.com/stm32mpu-ecosystem-v4/wiki/STM32_MPU_ecosystem_release_note#OpenSTLinux_-28Arm-C2-AE_Cortex-C2-AE-A7-29
I guess it is important to have TF-A, OpTee and uBoot versions aligned to our ecosystem releases.
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.