2025-06-19 11:54 PM
Good morning,
fairly new to this mpu family, I did a bit of a research but I'd like to get pointed to the correct procedure to, for instance, change bit 31 of RCC_SECCFGR.
This register would allow me for example to modify also PWR_CR1:BDP and PWR_CR2:MONEN registers/bits by unblocking PWR registers protection.
Assuming I'm working in a yocto/meta-st environment my first thought is to patch optee-os-stm32mp to modify that register and the PWR registers too since this kind of operations usually require secure context.
Question:
- Is there any easier approach, or high level approach (eg from uboot or kernel through SCMI) ?
Thanks in advance.
Solved! Go to Solution.
2025-06-20 7:02 AM
Well,
since i'm working with stm32mp135d, the simplest seems to patch and activate the tamper node in the optee-os device tree:
stm32mp131.dtsi:
tamp: tamp@5c00a000 {
compatible = "st,stm32mp13-tamp";
reg = <0x5c00a000 0x400>;
#address-cells = <1>;
#size-cells = <1>;
interrupts = <GIC_SPI 128 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&rcc RTCAPB>;
ranges;
st,backup-zones = <10 5 17>;
/* <INT_TAMPER_BKUP_DOMAIN_THRESHOLD TAMPER_CONFIRMED_MODE> */
st,tamp-internal-tampers = <1 1>;
then activate it inside stm32mp135d top level optee-os dts file:
&tamp {
status = "okay";
};
2025-06-20 7:02 AM
Well,
since i'm working with stm32mp135d, the simplest seems to patch and activate the tamper node in the optee-os device tree:
stm32mp131.dtsi:
tamp: tamp@5c00a000 {
compatible = "st,stm32mp13-tamp";
reg = <0x5c00a000 0x400>;
#address-cells = <1>;
#size-cells = <1>;
interrupts = <GIC_SPI 128 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&rcc RTCAPB>;
ranges;
st,backup-zones = <10 5 17>;
/* <INT_TAMPER_BKUP_DOMAIN_THRESHOLD TAMPER_CONFIRMED_MODE> */
st,tamp-internal-tampers = <1 1>;
then activate it inside stm32mp135d top level optee-os dts file:
&tamp {
status = "okay";
};
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.