2025-12-31 9:41 AM - edited 2025-12-31 9:42 AM
Hello,
I am using a STM32MP135F on a custom board which is working well using SD Card (sdmmc1).
The SDCard is partitioned as:
1) fsbl1
2) fsbl2
3) fip
4) bootfs
5) rootfs
From the SDcard system, I try to prepare the eMMC (4GB, sdmmc2).
I tried different configurations:
- mmcblk1p1boot0 (and boot1) contains fsbl1 (tf-a*.stm32), mmcblk1p1 contains fip => Could NOT find the fip partition! (although it contains the right GUID for fip partition 19...)
- mmcblk1p1boot0 contains fsbl1 (tf-a*.stm32) and fip (at offset 256KB => dd seek=512 bs=512) with
STM32MP> mmc partconf 1
EXT_CSD[179], PARTITION_CONFIG:
BOOT_ACK: 0x1
BOOT_PARTITION_ENABLE: 0x1 (boot0)
PARTITION_ACCESS: 0x0 (user)The BOOT_ACK is often erase and I have to renable it manually via u-boot on SDCard.
When I read back boot0 and boot1 at offset, the expected magic is present. Do you have an eMMC mapping for simple boot (the update & secure boot will be implemented later) to boot from eMMC successfully?
For information, please find the arguments for TFA:
EXTRA_OEMAKE:append:pn-trusted-firmware-a = " \
ARCH=aarch32 ARM_ARCH_MAJOR=7 \
AARCH32_SP=optee \
DTB_FILE_NAME=myb-stm32mp135x-512m.dtb \
STM32MP1_OPTEE_IN_SYSRAM=0 \
BL32=${DEPLOY_DIR_IMAGE}/optee/tee-header_v2.bin \
BL32_EXTRA1=${DEPLOY_DIR_IMAGE}/optee/tee-pager_v2.bin \
BL32_EXTRA2=${DEPLOY_DIR_IMAGE}/optee/tee-pageable_v2.bin \
BL33_CFG=${DEPLOY_DIR_IMAGE}/u-boot.dtb \
STM32MP_EMMC=1 \
STM32MP_SDMMC=1 \
STM32MP_EMMC_BOOT=1 \
BL33=${DEPLOY_DIR_IMAGE}/u-boot-nodtb.bin \
STM32MP13=1 \
STM32MP15=0 \
LOG_LEVEL=50 \
"
Thank you for your help and I wish you a happy new year!
2026-01-05 1:08 AM
Hi @RomainP
Not surer it could help, but please have a look to:
https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_code_overview#Boot_from_e-E2-80-A2MMC-E2-84-A2
https://wiki.st.com/stm32mpu/wiki/STM32_MPU_Flash_mapping#e-E2-80-A2MMC_memory_mapping
https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#e-E2-80-A2MMC
Regards
2026-01-23 6:59 AM
I think I have the same issue. I think the problem is the placement of image 2; BL32 aka u-boot. My current solution is to rebuilt the fib manually with --align 2048. I don't see any alignment options that can be set via the environment.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.