2023-01-06 10:48 AM
I've tried following the examples given here and here, but it will not work. I just want to enable a pull up resistor in the DTS file. Here is my DTS file. If anyone can please tell me why it's not working I would appreciate it.
/dts-v1/;
#include "stm32mp157.dtsi"
#include "stm32mp15xa.dtsi"
#include "stm32mp15-pinctrl.dtsi"
#include "stm32mp15xxac-pinctrl.dtsi"
#include "stm32mp15xx-dkx.dtsi"
&pinctrl {
button_pins_a: button-0 {
pins {
pinmux = <STM32_PINMUX('B', 12, GPIO)>;
bias-pull-up;
};
};
};
/ {
model = "STMicroelectronics STM32MP157A-DK1 Discovery Board";
compatible = "st,stm32mp157a-dk1", "st,stm32mp157";
chosen {
stdout-path = "serial0:115200n8";
};
button {
compatible = "test,button";
pinctrl-names="default";
pinctrl-0 = <&button_pins_a>;
status = "okay";
};
led {
extern-led {
compatible = "test,led";
gpios = <&gpiob 10 GPIO_ACTIVE_HIGH>;
linux,default-trigger = "cpu";
};
};
};
2023-01-09 9:12 AM
Hi scotty (Community Member)
GPIOs mappings are defined in the consumer device's node, in a property named
<function>-gpios, where <function> is the function the driver will request
through gpiod_get()
Also if the compatible field of DT doesn't match, nothing will happen.
So in your DT, you should add a prefix before "gpios", that is present in your driver.
ie: gpiod_get(&pdev->dev, "led", GPIOD_OUT);
led-gpios = <&gpiob 10 GPIO_ACTIVE_HIGH | GPIO_PULL_UP>;
Unless PB10 is already used by another instance.
Regards,
Olivier
2023-01-10 9:40 AM
@OlivierK
While this works for the LED, and indeed the pullup can be activated this way, I was asking how to make the button on the pinctrl work with a bias-pull-up. Please let me know how to configure it this was. Thank you.
2023-01-11 10:47 AM
Hi scotty (Community Member)
bias-pull-up or down should work the same for the button.
&pinctrl {
goodix_pins_a: goodix-0 {
pins {
pinmux = <STM32_PINMUX('F', 5, GPIO)>;
bias-pull-down;
};
}
root@stm32mp1:~# cat /sys/kernel/debug/pinctrl/soc:pinctrl@50002000/pinconf-pins | grep PF5
pin 85 (PF5): input - high - pull down
For button key, you can use also the gpio-keys driver.
joystick {
compatible = "gpio-keys";
pinctrl-0 = <&joystick_pins>;
pinctrl-names = "default";
button-0 {
label = "JoySel";
linux,code = <KEY_ENTER>;
interrupt-parent = <&stmfx_pinctrl>;
interrupts = <0 IRQ_TYPE_EDGE_RISING>;
};
Rgds,
Olivier
2023-01-12 10:16 PM
I understand now. I thought this device tree configuration would be immediately used on boot, but I must first load the LKM for the driver to instantiate these pins. Sorry for the confusion.
2023-01-17 9:25 AM
Hi scotty (Community Member)
Happy to read that this is clearer now.
Best Regards,
Olivier
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.