2019-12-17 11:57 AM
Im trying to integrate the firmware we have developed into our distribution on yocto. The documentation in the wiki [1] isn't really clear in how we add our own firmware to populate the MP1 coprocessor on boot. And the eample projects that the m4project.bb compiles seem to have a very rigid file structure compliant only with CubeMX. [2]
STM32 supports the Keil IDE we are wondering how we can use a project such as that in our yocto layer.
If anyone has succeeded in this endeavor please let us know.
[1]: https://wiki.st.com/stm32mpu/wiki/STM32CubeMP1_Package#Distribution_Package_for_STM32CubeMP1
2019-12-23 5:06 AM
Hi @RLeve
The layer meta-st/meta-st-stm32mp-addons/ is provided to ease integration of CubeMX generated project.
But today it support only SW4STM32 project structure.
Anyway you can also provide the .elf generated by Keil and manage to populate it to userfs and start it at boot.
Please look how this is done in m4projects recipe.
recipes-extended/m4projects/m4projects.inc
recipes-extended/m4projects/files/st-m4firmware-load-default.sh
A default m4 firmware defined in DEFAULT_COPRO_FIRMWARE can be loaded enabling the service "st-m4firmware-load.service" :
SYSTEMD_AUTO_ENABLE_${PN} = "enable"
Hope this help,
Olivier
2021-08-09 2:26 AM
Hi @Community member
I have created a STM32 project using STM32CubeIDE , i need to integrate Cortex-M4 firmware with distribution on yocto.
I copied the STM32CubeIDE project into PATH: openstlinux-5.10-dunfell-mp1-21-03-31/layers/sources/m4projects-stm32mp1/Projects/STM32MP157C-DK2/Examples and included in m4projects-stm32mp1.bb
But the file structure of examples in distribution is different from the STM32CubeIDE project.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.