2020-12-10 7:48 AM
Hello
I am trying to build an Image based on the Yocto Project for my stm32mp157c-DK2 according to st-wiki.
When I try to build the image I get the following error.
ERROR: Task do_populate_sdk in /home/mehdi/Distribution-Package/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb rdepends upon non-existent task do_package_write_deb in /home/mehdi/Distribution-Package/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb ERROR: Command execution failed: 1What did I miss or what did I do wrong in my local.conf file ?
Best regards.
I can share with you the content of the file.
2020-12-14 6:23 AM
Hi @SigmaPrime ,
st-wiki page you mention didn't cover any kind of customization but just building delivered image.
What are you trying to achieve ?
Where does this local.conf come from ?
Olivier
2020-12-14 7:06 AM
Thank you for your response Oliver.
I know. The wiki page is simply a basic support on how to build an image for my stm32.
I simply wanted to add some packages to be integrated into the build.
I don't understand why some packages are not able to be built properly although their recipes are in the layers provided by the wiki.
I simply want to learn how to configure my image based on the layers provided:
-Adding packages to be used
-Configuring the Linux Tree through menuconfig
I used to work with other distros like buildroot and the procedure to do these to steps was way less complicated than using Yocto (or a Yocto based project).
I am still learning that's why it is blurry in my mind.
The local.conf is located at ~/DP1/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1-disco/conf.
I simply used the IMAGE_INSTALL_append to add packages. It appears that this will not work with all packages.
Thank you.
2020-12-14 11:10 AM
I am not quite sure if I did it according to the proper way.
I will share my last version for the local.conf file.
For example "bluez" is not built in the final version of the image
When I flash my Image and go to the etc/ Directory it appears that not all Packages were installed although the layers containing the corresponding recipes are included
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.