STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP1 - I2C frequency too low

In my device tree, we config 400KHz, but on scope we see only ~ 50Hz, and the clock seems weird. Anyone know why? &i2c1 { pinctrl-names = "default", "sleep"; pinctrl-0 = <&i2c1_pins_a>; pinctrl-1 = <&i2c1_sleep_pins_a>; i2c-scl-rising-time-ns = <185>...

_legacyfs_online_stmicro_images_0693W00000bjEZXQA2.png
Dat Tran by Senior II
  • 2621 Views
  • 4 replies
  • 0 kudos

Resolved! STM32MP15x USART/UART Default Pins

Is stated on STM32MP157 datasheet's boot mode table that the MPU can be booted through UART: – USART2/3/6 and UART4/5/7/8 on default pins Nevertheless, I wasn't able to find which are the default pins for the UART interfaces, on the datasheet or refe...

Resolved! How to check, and eventually enforce Performance governor on STM32MP15 openst-linux?

I am trying to achieve hard real-time under 100us on the STM32MP157f-eval, specifically, on the Cortex A7 dual core.Note: I specifically target the Cortex A7 cores because the M4 is already taken for other tasks which requires much smaller latency.Wh...

A.M. by Associate III
  • 4901 Views
  • 7 replies
  • 0 kudos

HAL_SPI_Transmit times out

I have STM32CubeIDE Version: 1.12.0 and a STM32MP157F evaluation board.Created a M4 project and assigned SPI1 to it, generated the code.I then created a function to read a register:const uint16_t opcode = 0xe000; uint8_t value = 0; HAL_GPIO_WritePin(...

KBunn.1 by Associate II
  • 3305 Views
  • 6 replies
  • 0 kudos

DMA stops due to ADC Overrun

Hi,I have a problem with the DMA seemingly being shut down due to ADC overrun.What I want to achieve: Three ADC channels should be read indefinitely and the values should be written to memory by DMA as soon as they are ready.What's currently happenin...

RPape.1 by Associate II
  • 6388 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.