2025-09-18 10:38 PM
I created a layer using bitbake-layers create-layer --priority 7 ../layers/meta-st/meta-my-custo-layer and created
mkdir recipes-graphics/wayland/weston-init/ and created folder called files and append file weston-init_%.bbappend and in files i added my weston.ini where i disabled the panel=none and in bb append i added this code
FILESEXTRAPATHS:prepend := "${THISDIR}/files:"
SRC_URI:append = " file://weston.ini"
do_install:append() {
install -d ${D}${sysconfdir}/xdg/weston
install -m 0644 ${WORKDIR}/weston.ini ${D}${sysconfdir}/xdg/weston/weston.ini
}And added the layer using this bitbake-layers add-layer ../layers/meta-st/meta-my-custo-layer/
After that i built the image using bitbake st-image-weston but still it is taking the old weston.ini and the panel is visible
Can Someone help me on how to do it?
2025-09-22 12:01 AM
Hi @Sharan ,
Have you tried clearing your build folder before running the bitbake command again?
Next, you also need to check that there isn't another recipe that is built after the one you created , as these might overwrite your version of weston.ini
Regards,
Grégory
2025-09-22 12:58 AM
yes i used this command to clean bitbake -c clean weston-init and then used bitbake st-image-qt and then checked my appends using
sohum@sohum-aero:~/STM32MPU-Ecosystem1/Distribution-Package/build-openstlinuxweston-stm32mp15-disco$ bitbake-layers show-appends | grep weston-init
weston-init.bb:
/home/sohum/STM32MPU-Ecosystem1/Distribution-Package/layers/meta-st/meta-st-openstlinux/recipes-graphics/wayland/weston-init.bbappend
It is not showing my custom layer and i think its taking the default weston.ini file.Please give me the steps if i am wrong
2025-09-29 4:34 AM
It is showing my custom layer when i used bitbake-layers show-appends | grep weston
sohum@sohum-aero:~/STM32MPU-Ecosystem1/Distribution-Package/build-openstlinuxweston-stm32mp15-disco$ bitbake-layers show-appends | grep weston
NOTE: Started PRServer with DBfile: /home/sohum/STM32MPU-Ecosystem1/Distribution-Package/build-openstlinuxweston-stm32mp15-disco/cache/prserv.sqlite3, Address: 127.0.0.1:45383, PID: 416231
weston_11.0.1.bb:
/home/sohum/STM32MPU-Ecosystem1/Distribution-Package/layers/meta-st/meta-st-openstlinux/recipes-graphics/wayland/weston_11.0.1.bbappend
/home/sohum/STM32MPU-Ecosystem1/Distribution-Package/layers/meta-st/meta-my-custo-layer/recipes-graphics/weston/weston_11.0.1.bbappend
weston-init.bb:
/home/sohum/STM32MPU-Ecosystem1/Distribution-Package/layers/meta-st/meta-st-openstlinux/recipes-graphics/wayland/weston-init.bbappendI am able to store the image in /usr/share/weston/backgrounds but unable to change the Background image through bbappend file
FILESEXTRAPATHS:prepend := "${THISDIR}/files:"
# Background assets
DEFAULT_WESTON_BACKGROUND = "Sohum-Bg.png"
WESTON_HDMI_MODE ??= "1280x720"
SRC_URI:append = " \
file://weston.ini \
file://Sohum-Bg.png \
"
do_install:append() {
# Make sure weston config path exists
install -d ${D}${sysconfdir}/xdg/weston
install -d ${D}${datadir}/weston/backgrounds
rm -f ${D}${datadir}/weston/weston.ini
# Install your weston.ini
install -m 0644 ${WORKDIR}/weston.ini ${D}${sysconfdir}/xdg/weston
# Replace placeholders
sed -i -e "s:##DEFAULT_BACKGROUND##:${DEFAULT_WESTON_BACKGROUND}:g" \
-e "s:##HDMI_MODE##:${WESTON_HDMI_MODE}:g" \
${D}${sysconfdir}/xdg/weston/weston.ini
rm -f ${D}${datadir}/weston/backgrounds/ST*.png
# Install your background PNG
install -m 0644 ${WORKDIR}/${DEFAULT_WESTON_BACKGROUND} \
${D}${datadir}/weston/backgrounds/${DEFAULT_WESTON_BACKGROUND}
}
CONFFILES:${PN} += "${sysconfdir}/xdg/weston/weston.ini"
FILES:${PN} += " \
${sysconfdir}/xdg/weston/weston.ini \
${datadir}/weston/backgrounds/* \
"
Please help me on how to do the changes as it is not reflecting and it is taking the weston.ini and tried replacing also like it done for uboot its not working
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.