2026-03-25 10:42 AM
gpioinfo output
gpiochip9 - 10 lines:
line 0: "PZ0" input
line 1: "PZ1" input
line 2: "PZ2" input
line 3: "PZ3" input
gpiomon output
# gpiomon --num-events 1 --edges falling PZ0
^C
# gpiomon --num-events 1 --edges falling PZ1
^C
# gpiomon --num-events 1 --edges falling PZ2
^C
# gpiomon --num-events 1 --edges falling PZ3
gpiomon: unable to request lines on chip /dev/gpiochip9: No such device or address
why is there a problem with PZ3 pin specifically? noone is using it
should i add something in dts?
Solved! Go to Solution.
2026-03-26 12:29 AM
Hi @vdl
Most probable cause if because you already have another GPIO Px[3] defined as interrupt elsewhere.
This is a general constrains on most STM32 products due to the way the interrupt mux is done wrt GPIOs pins. Please refer to Reference Manual for details.
Regards.
2026-03-26 12:29 AM
Hi @vdl
Most probable cause if because you already have another GPIO Px[3] defined as interrupt elsewhere.
This is a general constrains on most STM32 products due to the way the interrupt mux is done wrt GPIOs pins. Please refer to Reference Manual for details.
Regards.
2026-03-26 12:57 AM
disabled emmc1 ( sd card interface ) which was using PD3 as interrupt - now PZ3 works
weirdly i still can gpiomon PD3 and other Px3 pins ( unused ones )
also i could gpiomon other Px3 before
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.