STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! cant put PZ3 into interrupt mode

gpioinfo outputgpiochip9 - 10 lines:line 0: "PZ0" inputline 1: "PZ1" inputline 2: "PZ2" inputline 3: "PZ3" inputgpiomon output# gpiomon --num-events 1 --edges falling PZ0^C# gpiomon --num-events 1 --edges falling PZ1^C# gpiomon --num-events 1 --edges...

vdl by Associate II
  • 233 Views
  • 2 replies
  • 0 kudos

Resolved! driving 1200x1920 screen

I'm in a bit of a pickle. I got a MIPI DSI screen with 1200x1920 resolution. It turns out for SMT32MP25x max vertical supported resolution is 1536. But datasheet says this.  Some over-target non-guaranteed use cases are possible, but with specific co...

vdl by Associate II
  • 405 Views
  • 3 replies
  • 0 kudos

Resolved! USB OTG FS in low power mode

Hi, I'm using a STM32MPU157C with linux 6.6, uboot, OP-TEE 4.0 and TF-A 2.10 and I have a Device Tree (for linux and uboot) which declares the USB OTG node as following : &usbotg_hs { compatible = "st,stm32mp15-fsotg", "snps,dwc2"; pinctrl-names = ...

CRA wiki links are broken

Several links on page about CRA are broken:https://wiki.st.com/stm32mcu/wiki/Security:Q%26A_for_CRA   https://wiki.st.com/stm32mcu/wiki/Security:Deep_dive_on_CRAFor this item, and in addition to solutions explained in (e), ST proposes several solutio...

Screenshot From 2026-03-18 15-26-35.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.