2020-05-01 4:48 PM
I have successfully built the st-example-image-qt using Bitbake (see first image) and have successfully downloaded it to the stm32mp157c-dk2 board (see second image). But now I cannot SSH into the board. When I use the ip add show eth0 command I can only see the inet6 ip and not inet. Then I tried to follow this article, https://wiki.st.com/stm32mpu/wiki/How_to_perform_ssh_connection, but there is no /etc/init.d/sshd directory and I can't use apt install as I have no wifi connection on the board. Anyone else have this issue with the qt example image?
EDIT 1: I also tried this article with no luck although now I do see an inet IP address when I manually set it with the ifconfig command I still can't SSH in, https://wiki.st.com/stm32mpu/wiki/How_to_configure_ethernet_interface. More information, I am using an Ubuntu virtual box as my host computer and using a usb 3 ethernet to USB adapter so not sure if that has anything to do with it? I did try this on a native linux computer with an ethernet port and got the same results.
EDIT 2: I got the ssh to work if I plug the board directly into my router but still won't work with ethernet plugged from board directly to computer.
2020-05-06 7:31 AM
Hello,
Recently ssh server moved from openssh to dropbear, so that's why the wiki article is not updated (sorry for that). It will be done shortly but it won't change your issue.
I did make a trial on my side on ubuntu 18.4 with a home gateway (both DK2 and host PC connected to the gateway) and it works fine:
stmcust@stmcust-HP-EliteBook-840-G5:~/v1.2.0/$ ssh root@192.168.1.78
The authenticity of host '192.168.1.78 (192.168.1.78)' can't be established.
RSA key fingerprint is SHA256:Jm+8xJJgh3RlrtX/t32/+i+nuZQlYIPsqh0+9NALkgM.
Are you sure you want to continue connecting (yes/no)? yes
Warning: Permanently added '192.168.1.78' (RSA) to the list of known hosts.
root@stm32mp1:~# systemctl | grep drop
dropbear@3-192.168.1.78:22-192.168.1.71:43846.service loaded active running SSH Per-Connection Server (192.168.1.71:43846)
dropbearkey.service loaded active exited SSH Key Generation
system-dropbear.slice loaded active active system-dropbear.slice
dropbear.socket loaded active listening dropbear.socket
root@stm32mp1:~#
As you can see a systemd service is started at every ssh connection to the dropbear server, you should see it.
Then if the static connection is not working:
2020-05-06 7:38 AM
Board $> ls /lib/systemd/network
50-wired.network 52-static.network.static 80-container-vz.network
50-wired.network.static 80-container-host0.network 99-default.link
51-wireless.network.sample 80-container-ve.network
52-static.network.static:
[Match]
Name=eth0
[Network]
DNS=192.168.72.254
Address=192.168.72.2/24
Gateway=192.168.72.254
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.