STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Optimization boot time

Hi! I am following the tutorial How to optimize the boot time for stm32mp157c-ev1 I have enabled FastMap but the time is not reduce (about 10s to attaching ubi) I want to avoid attaching ubi... Is it posible load kernel and device tree in nand using ...

AVazquez by Associate III
  • 887 Views
  • 0 replies
  • 0 kudos

Crypto API

Trying to build image using unmodified distribution package. Hardware crypto devices are enabled in config:root@stm32mp1:/etc# zcat /proc/config.gz | grep CONFIG_CRYPTO_DEV_STM32CONFIG_CRYPTO_DEV_STM32_CRC=yCONFIG_CRYPTO_DEV_STM32_HASH=yCONFIG_CRYPTO...

FreeRTOS memory issue

Hello,I use STM32MP157C-DK2 board with freeRTOS.I run my bord in engeneering mode with default freeRTOS parameters provided by cubeMXI create tree threads in my application but the last does not start.May be it is a memory space problem. So I try to ...

ABous.1 by Associate III
  • 1142 Views
  • 1 replies
  • 0 kudos

Poor OpenGL performance

I've run a simple graphical program with Mono and OpenTK. It contains a simple fragment shader (demo). One frame renders about 7 seconds and CPU usage is 100%. Is it normal?vec2 p = ( gl_FragCoord.xy / resolution.xy ) - 0.5; float sx = (amp)*1.9 * si...

I would like to knew why the GPIO-Pin PA11 is on high level while the Board boots. I configured the Pin Muxing with CubeMx and Loaded the Device tree for the Kernel in the boot directory and synced it. I configured the pin as a PWM pin.

When I run my M4 Application every thing is working fine. But while the Board boots until i start the M4 remoteproc the pin is on high level. How can I set the pins reset(boot) configuration to low? I'am using the developer package.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.