STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP157dk uboot ums seen in virtualbox Macos, bootfs, vendorfs etc. are a read only file systems

Having doing a workshop regarding OpenST linux boot customisation (https://www.youtube.com/watch?v=hqGA5Krk0mU), I stumbled on a problem with a mass storage mount. Doing "ums 0 mmc 0" in uboot gives me partitions within an sdcard but only to see them...

michh by Associate
  • 3061 Views
  • 2 replies
  • 1 kudos

Remoteproc start process

Hi Im using a STM32MP157-DK2 with a OpenSTlinux. I load my .elf file of for the M4 to /lib/firmware/ and starts it by chaning the state to start in remoteproc. The problem I have is that remoteproc seems to not run the code from the beginning of the ...

carer by Associate
  • 1724 Views
  • 0 replies
  • 0 kudos

Resolved! FreeBSD Port for mp157C

Hello! Is it feasible to start FBSD kernel?So far I stuck with following error (seems to be from tf-a):  Loading kernel... /boot/kernel/kernel text=0x1b4 text=0x5ad698 text=0x17e3d0 data=0xa4860 data=0x0+0x20c000 0x4+0x88d70+0x4+0xea43b| Loading conf...

ptpd support for Linux on STM32MP133A

The STM32MP133A supports Linux, and has PTP support in its ethernet peripheral. However, there doesn't seem to be a driver, or port of ptpd for that specific hardware.The peripheral seems similar to other STM32 parts for which there are community por...

qua by Senior
  • 2291 Views
  • 2 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.