STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FreeBSD port in progress

Hello! Although, the OS is not supported, I'd be happy to get any clues on my relatively generic question.I have realized, that TEX remapping registers  (PRRR and NMRR) values are hardcoded in Linux kernel source..equ NMRR, 0x40e040e0I'm particularly...

Resolved! Optee permission errors

I'm having trouble in bringing up my custom board. I've made a custom device tree using CubeMX and adding the sections as described in "Lab-MP15_FromPartNumber_To_BasicDeviceTree_with_CubeMx". I can program fsbl-boot and fip-boot, but i'm not able to...

Resolved! Cross compiling pyzmq

I've been trying to cross compile pyzmq for my stm32mp135f-dk and I'm facing issues with it. I've ran the script to setup my environment for the SDK. And made the required changes in the setup file. Here's my stackoverflow post with the logs as well....

Resolved! Troubles with linking custom application arm-ostl-linux-gnueabi-gcc for STM32MP157x-DK2

Hi, I tried the Hello World application on Cortex-A7, I want to try linking my custom application library in this example. Can I do that?I changed the print_hello function and calling another function from my custom library.I tried linking custom lib...

btank by Associate II
  • 2225 Views
  • 1 replies
  • 0 kudos

Hello, I want to enable SPI4 but just get a timeout. My SOM is based on STM32MP157, use Linux 5.10 Main line. I connected a logic analyser and see the pins are set to high a soon linux was booted. I dont see any clock impulses.

My device tree:spi4_pins_csa: spi4-0 { pins { pinmux = <STM32_PINMUX('E', 12, AF5)>, /* SPI4_SCK */ <STM32_PINMUX('E', 14, AF5)>; /* SPI4_MOSI */ bias-disable; drive-push-pull; slew-rate = <1>; }; pins2 { pinmux = <STM32_PI...

Wechmarer by Associate II
  • 2449 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.