2023-10-24 4:13 AM - edited 2023-10-24 4:13 AM
The STM32MP133A supports Linux, and has PTP support in its ethernet peripheral. However, there doesn't seem to be a driver, or port of ptpd for that specific hardware.
The peripheral seems similar to other STM32 parts for which there are community ports of ptpd, but
a) not officially supported
and
b) for FreeRTOS, not Linux.
Has anyone used ptpd with a STM32MP133A and Linux? Does ST support it at all?
2023-10-24 4:57 AM
Hi @qua ,
I'm not expert and not sure what you mean by PTPd, but PTP looks to be supported in stmmac driver.
* On gmac4 specifically:
* Enable SYNC, Pdelay_Req, Pdelay_Resp when TSEVNTENA is enabled.
* or
* Enable SYNC, Follow_Up, Delay_Req, Delay_Resp, Pdelay_Req, Pdelay_Resp,
* Pdelay_Resp_Follow_Up if TSEVNTENA is disabled
SNAPTYPSEL TSMSTRENA TSEVNTENA -> 01 0 1
in /driver/net/ethernet/stmicro/stmmac_main.c
* stmmac_hwtstamp_set - control hardware timestamping.
static int stmmac_hwtstamp_set(struct net_device *dev, struct ifreq *ifr)
...
case HWTSTAMP_FILTER_PTP_V2_EVENT:
/* PTP v2/802.AS1 any layer, any kind of event packet */
config.rx_filter = HWTSTAMP_FILTER_PTP_V2_EVENT;
ptp_v2 = PTP_TCR_TSVER2ENA;
snap_type_sel = PTP_TCR_SNAPTYPSEL_1;
if (priv->synopsys_id < DWMAC_CORE_4_10)
ts_event_en = PTP_TCR_TSEVNTENA;
...
root@stm32mp1:~# ethtool -T eth0
Time stamping parameters for eth0:
Capabilities:
hardware-transmit
software-transmit
hardware-receive
software-receive
software-system-clock
hardware-raw-clock
PTP Hardware Clock: 0
Hardware Transmit Timestamp Modes:
off
on
Let me know if this help
Olivier
2023-10-24 5:00 AM
Thank you Oliver, that is very helpful. I will get hold of a dev board and try it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.