STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Kernel cannot find the rootfs

Hello,I have a custom board based on STM32MP151c with an eMMC on it (no SD card). The eMMC is successfully found in the U-Boot and has the following partitioning:part list mmc 0   Partition Map for MMC device 0 -- Partition Type: EFI   Part Sta...

alenik-mm by Associate II
  • 4184 Views
  • 5 replies
  • 0 kudos

HSEM read lock vs write lock?

Hi!So I was reading the wiki here https://wiki.st.com/stm32mpu/wiki/How_to_configure_system_resourcesand they tell you to use PERIPH_LOCK, which is a function that can be found here:https://github.com/STMicroelectronics/STM32CubeMP1/blob/1.3.0/Projec...

STM32MP1 FDCAN 1 or 2 not working

I am configured both the FDCAN interfaces on the STM32MP1 discovery board with the settings below using STM32CubeMX. FDCAN1: PA11 (RX) PA12 (TX)FDCAN2: PB12 (RX) PB13 (TX)But I can't seem to get any data from either interface. I have a logic analyzer...

ASuar.1 by Associate III
  • 2733 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.