STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! UBoot SPL DDR Testing on STM32MP157FAD1 error stm32mp1_clk_get_id: clk id 142 not found

I am building uboot spl for DDR testing of a custom board based on the STM32MP157FAD1 MPU. The design uses I2C6 to communicate with the PMIC. The following error occurs: "stm32mp1_clk_get_id: clk id 142 not found". Any suggestions on why the I2C6 clo...

TStru.1 by Associate II
  • 4893 Views
  • 8 replies
  • 0 kudos

Resolved! MMC Device 0 not found

Hello,I have a custom board with an eMMC on it and with no SD card available. In the U-Boot device tree I have the following line (On sdmmc2 is my eMMC):aliases{ mmc0 = &sdmmc2; };The U-Boot seems to partly have a problem with it. ​Commands like "mm...

alenik-mm by Associate II
  • 6240 Views
  • 4 replies
  • 0 kudos

IPCC when freeing Channel

Hi,i have a question regarding to the IPCC Communication and the OPENAMP_check_for_message(); function. For example iam sending data from A7 to the M4. So the A7 will cause an RXO Interrupt at the M4. Now my Question ist when this Interrupts is clear...

YRink.1 by Associate II
  • 2557 Views
  • 3 replies
  • 0 kudos

Mainline Linux fails to set up FS OTG

Hi there,After following this tutorial (and updating the compatible string): https://wiki.st.com/stm32mpu/wiki/OTG_device_tree_configurationI've managed to create a patch that adds these nodes to my device tree:... +&usbphyc { + status = "okay"; +}; ...

JGuy1 by Associate II
  • 3065 Views
  • 3 replies
  • 0 kudos

Resolved! What will be the correct steps to modify the dts file (stm32mp157a-dk1.dts) and deploy to the deploy/images for flashing to sdcard

My goal is to add i2c5 in the dts for userspace access however it is not visible at /sys/bus/i2c/devices. My steps are as follows:1) bitbake virtual/kernel -c devshell2) in new shell, modify the arch/arm/boot/dts/stm32mp157a-dk1.dts3) in new shell, m...

JLeun.1 by Associate
  • 2118 Views
  • 2 replies
  • 0 kudos

gcnano-binaries 6.4.3 broken

Hello,will there be updates to the gcnano-binaries?The latest version (6.4.3) seems to be broken.When trying to start the cog browser (wpewebkit based) it crashes on eglCreateWaylandBufferFromImageWL.After reverting to gcnano 6.4.1 it is working agai...

Artem by Associate III
  • 3689 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.