2021-01-04 10:24 PM
I have modified STM32MP157C-DK2 board with NAND flash connected through FMC and it works properly with linux kernel 5.4-stm32mp-r1. I notice that there are some changes to FMC in 5.4-stm32mp-r2 and tried to build my custom linux using the newer release. Unfortunately, the kernel always crashed because it can't open the MTD device. The device can boot TF-A and u-boot properly but it always stuck at the kernel.
in 5.4-stm32mp-r1 version I only modify the DK2 device tree by stripping unused nodes, removing nodes that use the same pin as FMC, and adding FMC node by copying the configuration from stm32mp15xx-evx.dtsi. I use the same approach in 5.4-stm32mp-r2 as I assume the configuration from stm32mp15xx-evx.dtsi is enough to make the device boot from NAND.
[ 1.158408] UBI error: cannot open mtd UBI, error -2
[ 1.162737] stm32_rtc 5c004000.rtc: setting system clock to 2000-01-16T08:50:47 UTC (948012647)
[ 1.173134] VFS: Cannot open root device "(null)" or unknown-block(0,0): error -6
[ 1.179147] Please append a correct "root=" boot option; here are the available partitions:
[ 1.187592] 0100 65536 ram0
[ 1.187596] (driver?)
[ 1.193642] 0101 65536 ram1
[ 1.193645] (driver?)
[ 1.199654] 0102 65536 ram2
[ 1.199657] (driver?)
[ 1.205750] 0103 65536 ram3
[ 1.205754] (driver?)
[ 1.211906] 0104 65536 ram4
[ 1.211910] (driver?)
[ 1.217898] 0105 65536 ram5
[ 1.217901] (driver?)
[ 1.223980] 0106 65536 ram6
[ 1.223983] (driver?)
[ 1.230269] 0107 65536 ram7
[ 1.230273] (driver?)
[ 1.236141] 0108 65536 ram8
[ 1.236144] (driver?)
[ 1.242243] 0109 65536 ram9
[ 1.242246] (driver?)
[ 1.248303] 010a 65536 ram10
[ 1.248306] (driver?)
[ 1.254473] 010b 65536 ram11
[ 1.254476] (driver?)
[ 1.260653] 010c 65536 ram12
[ 1.260656] (driver?)
[ 1.266808] 010d 65536 ram13
[ 1.266811] (driver?)
[ 1.272977] 010e 65536 ram14
[ 1.272980] (driver?)
[ 1.279144] 010f 65536 ram15
[ 1.279147] (driver?)
[ 1.285319] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
[ 1.293566] CPU: 0 PID: 1 Comm: swapper Not tainted 5.4.56 #1
[ 1.299293] Hardware name: STM32 (Device Tree Support)
[ 1.304450] [<c010d5e0>] (unwind_backtrace) from [<c010b01c>] (show_stack+0x10/0x14)
[ 1.312163] [<c010b01c>] (show_stack) from [<c0116e08>] (panic+0x114/0x2fc)
[ 1.319118] [<c0116e08>] (panic) from [<c0901318>] (mount_block_root+0x248/0x2f8)
[ 1.326586] [<c0901318>] (mount_block_root) from [<c0901718>] (prepare_namespace+0x180/0x1c4)
[ 1.335097] [<c0901718>] (prepare_namespace) from [<c06157d8>] (kernel_init+0x8/0x110)
[ 1.343003] [<c06157d8>] (kernel_init) from [<c01010e8>] (ret_from_fork+0x14/0x2c)
[ 1.350551] Exception stack(0xc7033fb0 to 0xc7033ff8)
[ 1.355594] 3fa0: 00000000 00000000 00000000 00000000
[ 1.363763] 3fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 1.371927] 3fe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 1.378534] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0) ]---I have another DK2 board without any modification and the kernel runs without any problem
2021-01-11 2:52 AM
Hi @jandriea ,
Moving to 5.4-stm32mp-r2 did you also upgradre TF-A and U-boot with V2.1 version ?
It's recommended to be consistent and not mix element from various deliveries.
Olivier
2021-01-11 11:38 PM
Hi @Community member
Thanks for your response. I am pretty sure that I also upgrade the TF-A and U-Boot as I clone the meta-st-stm32mp layer from STMicroelectronis github site and checked out openstlinux-5.4-dunfell-mp1-20-11-12 tag.
The bootloader runs properly as it can run from NAND and I can load the zImage and kernel device tree from U-Boot. The problem only occurred when the kernel is already loaded. As I search on another site, someone mentioned that the problem is the kernel didn't detect NAND flash. Thus, the kernel failed to load the UBI volume
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.