STM32 MCUs
From FAQs to complete How-to articles, find useful articles on STM32 MCUs programming, troubleshooting, ecosystem, and product details.
cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge base articles

Custom signal generation using PWM and DMA

Introduction The purpose of this article is to explain how to generate a custom signal, a sine wave in this case, using an STM32 Microcontroller’s DMA controller and a PWM output from a timer. Although this example uses the NUCLEO-H745ZI-Q, the same ...

1683.png 1685.png 1687.png 1690.jpg

Implementing debug authentication on STM32H5 using CLI tools

Introduction Debug authentication is a critical security feature of the system considering that with a debugger the user can access a large part of the system. To control a reopening of the debug port, the device imposes a debug authentication proto...

RuchitN_0-1703203603049.png RuchitN_1-1703203603051.png RuchitN_2-1703203603053.png RuchitN_3-1703203603055.png
Ruchit N by ST Employee
  • 8364 Views
  • 4 comments
  • 3 kudos

Setting clock multipliers and dividers for the STM32H5

Introduction  Clock configuration is a fundamental aspect of microcontroller (MCU) design, directly influencing the performance and power consumption of the system. In the STM32 series, the reset and clock control (RCC) peripheral manages the system...

Capture d’écran 2025-03-25 111404.png Clock configuration.png cycle to cycle jitter.png PLL power consumption.png
Sarra.S by ST Employee
  • 2368 Views
  • 0 comments
  • 2 kudos

STM32N6 low-power modes and Standby demo

Summary This article provides an overview of the low-power modes available in the STM32N6 series. It provides hands-on instructions for utilizing the Standby demo, detailing how RAM retention is implemented and how to run the demo code. Introduction...

BMontanari_0-1741202262411.png BMontanari_1-1741202262414.png BMontanari_2-1741202262417.png BMontanari_3-1741202262423.png

How to calibrate the STM32's real-time clock (RTC)

Summary This article provides a step-by-step guide on how to calibrate the precision of a real-time clock (RTC). The examples in this guide are provided using the NUCLEO-U575ZI-Q board, but can be tailored to any other STM32. Introduction The real-t...

BMontanari_1-1732041172104.png BMontanari_2-1732041172109.png BMontanari_3-1732041172111.png BMontanari_4-1732041172112.png

Injecting and handling ECC errors in STM32H7 RAM

Summary This article provides a step-by-step method to test the ECC single and double errors in the STM32H7 series. Find attached to the article a ECC RAM project for testing purposes.  Introduction In STM32H7 microcontrollers, RAM ECC (Error Correc...

CMYL_0-1730289954134.png CMYL_1-1730290944180.png CMYL_2-1730291031740.png CMYL_3-1730291031742.png
CMYL by ST Employee
  • 4897 Views
  • 1 comments
  • 4 kudos

STM32H7 series spread-spectrum clock generation (SSCG)

Summary The main objective of this article is to present the STM32H7 spread-spectrum clock generation (SSCG) feature. STM32H7 differs from other series by using PLL fractional with Timer/DMA.  For an overall introduction to spread-spectrum clock gen...

StassenC_2-1721652053910.png StassenC_3-1721401647084.png StassenC_8-1721401647157.png StassenC_7-1721401647130.png
Stassen.C by ST Employee
  • 6307 Views
  • 5 comments
  • 2 kudos

How to use FileX with eMMC for file system management

Summary This article guides you on how to use FileX, a fully compliant FAT library for media storage and file system management with eMMC. In this example, the selected hardware is an STM32U5A9-DK board featuring anintegrated eMMC card readily availa...

BMontanari_0-1706718933631.png BMontanari_1-1706718933638.png BMontanari_2-1706718933639.png BMontanari_3-1706718933642.png

How to utilize STM32 system (ROM) bootloader commands

1. System (ROM) bootloader The system bootloader is present on all STM32 MCUs. As the name suggests, it is located on the system memory (ROM) area of the MCU. The system bootloader is located on the read only portion of the memory and is programmed ...

AMEMCUSM_0-1699295709220.png AMEMCUSM_1-1699295709234.png AMEMCUSM_0-1699997045423.png AMEMCUSM_3-1699295709381.png

How to connect an STM32WB server to multiple clients

The STM32WB as a server can be connected to 8 clients max for the STM32WB3x and STM32WB5x.In contrast, 5 clients max for the STM32WB1x using the stm32wbxx_BLE_Stack_full_fw.bin stack (from STM32CubeWB version 1.21.0). To achieve this, the server nod...

STTwo-32 by ST Employee
  • 1063 Views
  • 0 comments
  • 1 kudos

How to implement the USB device composite class USB DFU + HID

Introduction This article is a step-by-step guide on how to implement an STM32 application as a USB device. This device should combine human interface device (HID) and device firmware upgrade (DFU) functionalities into a composite USB device. This al...

FBL_0-1737475963279.png FBL_0-1740648445294.png FBL_1-1737475963161.png FBL_2-1740682200093.png
FBL by ST Employee
  • 6356 Views
  • 0 comments
  • 1 kudos