on
2021-12-16
12:09 AM
- edited on
2025-11-26
5:33 AM
by
Laurids_PETERSE
After programming my STM32H7/STM32H7RS and performing a reset, I find that I can no longer connect to my target using STLINK. Why does this happen? How can I recover my board?
Note that your STM32H7/STM32H7RS’s SMPS or LDO firmware power configuration must match with the board’s hardware configuration. If not, you will face a deadlock situation such that after the reset the STLINK can no longer be used to connect to the target.
The firmware’s power configuration is located in the main.c file, namely in the function SystemClock_Config(). Depending on your target’s hardware power configuration, modify your SystemClock_Config function to use the corresponding line of code:
1. Direct SMPS Hardware Power Configuration
/*!< Supply configuration update enable */ HAL_PWREx_ConfigSupply(PWR_DIRECT_SMPS_SUPPLY);
2. LDO Hardware Power Configuration
/*!< Supply configuration update enable */ HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
If at any time a deadlock situation is faced due to a mismatch between the target’s hardware power configuration and firmware setting, you can recover the board by doing the following:
Step 1. Power off the board
Step 2. Locate the BOOT0 pin and connect the BOOT0 pin to VDD using a wire. This pulls the BOOT0 pin to HIGH, which changes the device’s boot address to start the bootloader in system memory instead of booting from the target’s flash memory (which currently houses the firmware that is setting the incorrect SMPS/LDO configuration).
Step 3. Power on the board and connect to the target using STM32CubeProgrammer.
Step 4. Perform a mass erase.
Step 5. Power off the board and remove the wire between BOOT0 and VDD.
Step 6. The recovery is now completed; you can once again connect to the target using the STLINK and use the board as normal.
For additional information on this warning, please refer to UM2408, in specific the section concerning Internal SMPS / LDO Configuration.
This answer helped to me, thank you very much.
Please note that: before do this, be ensure that your VDDA should not be floating. if your VDDA pin is floating, please connect with a dupont/jumper cable to VDD or 3.3V.
Very helpful, thank you. I wasted more than an hour trying to get the Programmer to connect to my board, this procedure is quick, easy and very effective.
One question to this process: Before I started, I checked my VDD port and it is at 0.0V...shouldn't it be at high already? Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.